|
QUESTION:
How can one uninstall older versions of Sinvert Select?
ANSWER:
De-installation of Sinvert Select is carried out via following procedure:
Start -> Settings -> Control Panel -> Software -> Remove Software
Open Windows Explorer and navigate to the SINVERT Select installation path.
As default SINVERT Select is installed under:
C:\Program Files\Siemens\SINVERT Select
resp.
C:\Programme\Siemens\SINVERT Select
If there exists a SINVERT Select folder, delete this folder along with all its subdirectories.
Notice: If you delete this folder all the data in the directories concerned will be lost.
If necessary back up any required data beforehand!
|