show the entry list
Delivery Release: SIMATIC powerrate V3.0 SP1
Part number:
Summary Internet document

With immediate effect, SIMATIC powerrate V3.0 SP1 is available for delivery. As a separate product and full version, SIMATIC powerrate V3.0 SP1 replaces its immediate predecessor, SIMATIC powerrate V3.0. The sale of SIMATIC powerrate V3.0 ends with the availability of SIMATIC powerrate V3.0 SP1.    

SIMATIC powerrate V3.0 SP1 can be requested as a free download to the previously available version SIMATIC powerrate V3.0 from the download area of the SIMATIC Customer Support Website (see entry ID: 42005963). An automatic sending of the service pack on account of a previous hotfix delivery does not occur.

Internet document Summary


1. Contents

Compared to SIMATIC powerrate V3.0 (see entry ID: 38823708), the following changes regarding delivery scope and application apply: 

  • The number of configurable rate zones was increased from 6 to 12.
     
  • Starting with V3.0 SP1, the SIMATIC powerrate Engineering and Upgrade packages also include a license for SIMATIC WinCC/User Archives. This license is required for the use of the load management and the batch reports.  
     
  • SIMATIC powerrate is released for the use with: 
    • WinCC/Web Navigator or PCS 7 Web Server / Client
    • WinCC/Redundancy (in connection with S7-400) or PCS 7 OS Redundancy

Recommendation for SIMATIC WinCC powerrate:

  • WinCC configuration integrated with STEP 7
  • Use of BPC (Basic Process Control)

2. Ordering Data

SIMATIC powerrate V3.0 SP1
  WinCC PCS 7
Trial License (for 30 days) 3ZS2795-1CC30-0YG7 3ZS2785-1CC30-0YG7
Engineering + AS Runtime (unlimited) 3ZS2795-1CC30-0YG0 3ZS2785-1CC30-0YG0
Upgrade V 2.0 -> V 3.0 SP1
Engineering + AS Runtime (unlimited)
3ZS2795-1CC30-0YE0 3ZS2785-1CC30-0YE0

 Entry ID:42025928   Date:2010-04-19 
I regard this article....as helpfulas not helpful                                 
related links
Service Pack 1 (Update) for SIMAT ...
Hotfix 1 (Update) for SIMATIC pow ...
Hotfix 2 (Update) for SIMATIC Win ...
Why are reports not created autom ...
How do you use SIMATIC powerrate ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour