show the entry list
3RA2 Function Modules: Surge suppression incorporated in the function modules 3RA27 and 3RA28?
Part number:

QUESTION:

Which measures for surge suppression have been taken on the function modules 3RA27 and 3RA28?

 

 

ANSWER:

All function modules 3RA27 and 3RA28 are off factory equipped with integrated varistor for surge suppression.

For the wye-delta function module, which consists of one basic module and two coupling modules, the following applies:
The basic module comes from factory with integrated varistor.

In the circuit of the basic module for wye-delta starting, a varistor is already factory assembled.

Through parallel connected energizing of the contactor coils by means of plugging the connecting cables the surge suppression of the three subsidiary contactors (line, delta, wye) is established.

 

 Entry ID:42002333   Date:2012-06-28 
I regard this article....as helpfulas not helpful                                 
related links
System Manual Industrial controls ...
Manual SIRIUS Function Modules fo ...
ET 200X and SF-LED for load volta ...
3RT19/3RT29 Accessories and Spare ...
3RF: Memory with 3RF29 function m ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour