show the entry list

WinAC MP -- Product information -- Technical data and ordering information 
Is WinAC MP 2008 compatible with Windows 7? 
What are the requirements for using the S7 routing function and which modules can you implement? 

Is WinAC MP 2008 compatible with Windows 7?Go to beginning
Part number:

Description
WinAC MP 2008 is released for WinCC flexible 2008 SP2 and Windows XP.
WinAC MP2008 is not released for and cannot be installed in Windows 7.

Keywords
OS, Operating System, Soft PLC, C7, Panel, PLC, Multipanel, PLC software

What are the requirements for using the S7 routing function and which modules can you implement?Go to beginning
Part number:

Description
From STEP 7 V5.0 SP3 HF3 onwards you can reach ST stations online over and beyond subnet limits with the PG/PC, in order, for example, to load user programs or a hardware configuration or in order to execute test and diagnostic functions. You can connect a PG/PC at any place within the network and connect online to any stations which are reached through gateways.

Gateway
The gateway from a subnet to one or more other subnets is in a SIMATIC station that has interfaces to the subnets concerned.

Requirements

  • At least STEP 7 V5.0 SP3 HF3 is installed on the PG/PC for configuration and use of the S7 routing function.
  • An interface (Industrial Ethernet or PROFIBUS PC CP) is installed in the PG/PC to establish a connection to the gateway. You can use PROFIBUS PC CPs 55xx and 56xx. You can use any NDIS-compatible Ethernet network card (3COM, CP1613, for example) as Industrial Ethernet interface in the PG/PC.
  • The associated communications modules of the station support the S7 routing function.
  • The network configuration does not go across project boundaries.
  • Both the modules and the PG or PC are loaded with the configuration information that contains the latest "knowledge" about the complete network configuration of the project.
    Technical background
    All the modules associated with the gateway must receive information about which subnets can be reached over which routes (= routing information).

Note
The lists below have been updated with the modules of the hardware catalog of STEP 7 V5.4 SP2. This means that older modules which support the S7 routing function are listed in the tables, but are not necessarily included in the hardware catalog of the latest versions of STEP 7.

SIMATIC S7-CPUs
The list below gives an overview of the SIMATIC S7 CPUs that support the S7 Routing function.

584459_Overview_CPUs_en.pdf ( 43 KB )

Communications processors (CPs)
The list below gives an overview of the PROFIBUS and Industrial Ethernet CPs that support the S7 Routing function.

584459_Overview_CPs_en.pdf ( 41 KB )

SIMATIC S7 FM modules
The list below gives an overview of the SIMATIC S7 FM modules that support the S7 Routing function.
 

FM

Version

Order number

FM 356-4 V5.0 V5.0 6ES7356-4BM00-0AE0
FM 356-4 V5.0 V5.0 6ES7356-4BN00-0AE0
FM 456-2 V5.0 6ES7456-2AA00-0AB0
Table 01

Gateways
The list below gives an overview of the gateways that support the S7 Routing function.
 

Link

Version

Order number

IE/PB Link as from V1.0 6GK1411-5AA00
IE/PB Link PNIO as from V1.0 6GK1411-5AB00
IWLAN/PB Link PNIO as from V1.1 6GK1417-5AB00
IWLAN/PB Link PNIO as from V1.1 6GK1417-5AB01
Table 02

SIMATIC S7 IM modules
The list below gives an overview of the SIMATIC S7 IM modules that support the S7 Routing function.
 

IM

Version

Order number

IM 467 as of V2.0 6ES7467-5GJ02-0AB0
IM 467 FO as of V2.0 6ES7467-5FJ00-0AB0
Table 03

SIMATIC WinAC RTX, WinAC Slot and WinAC MP
The list below gives an overview of SIMATIC WinAC RTX, WinAC Slot and WinAC MP that support the S7 Routing function.
 
WinAC Version Order number
WinAC RTX as from V4.0 6ES7671-0R...
WinAC Slot 412 as from V3.2 6ES7673-2C...
WinAC Slot 416 as from V3.2 6ES7673-6C...
WinAC MP as from V4.1 6ES7671-4EE00-0YA0
6ES7671-5EF01-0YA0
6ES7671-7EG01-0YA0
Table 04

SINAUT communications modules
The list below gives an overview of SIMATIC WinAC RTX, WinAC Slot and WinAC MP that support the S7 Routing function.
 
TIM Version Order number
TIM 3V-IE as from V1.0 6NH7800-3BA00
TIM 3V-IE Advanced as from V1.1 6NH7800-3CA00
TIM 4R-IE as from V1.0 6NH7800-4BA00
TIM 4RD as from V3.x 6NH7 800-4AD90
Table 05

Note
The target station does not have to support the S7 Routing function.

Additional Keywords
Module function

 Entry ID:41767521   Date:2012-12-13 
I regard this article....as helpfulas not helpful                                 






























related links
Which modules can you use when im ...
What are the requirements for usi ...
SIMATIC S7-300 Instruction list S ...
What is multicomputing mode and w ...
How many communication instances ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour