show the entry list
PROFINET general -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
How can you standardize and destandardize analog values with STEP 7 V5.5?
How do you configure a shared device when you are using a CPx43-1 Advanced as PROFINET IO controller and the GBIT interface of the module is networked?
What should you watch out for when you configure the I device and the higher-level IO controller in the same STEP 7 project?
How do you configure the SIMATIC MV440 / MV420 code reader device with STEP 7 (TIA Portal) as a PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
How do you reset the IP address and device name of an I device?
What should you watch out for when parameterizing the watchdog time when a ring redundancy is established with the Media Redundancy Protocol?
What should you watch out for in the configuration when data is exchanged via Industrial Ethernet in parallel via I/O addresses and TCP and UDP connections?
How do you configure the SIMATIC MV440 code reading system as PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
Assigning names and addresses in PROFINET IO
Which options are available for configuring the ET 200 stations?
How do you connect the SIMATIC Field PG to the bus system to parameterize and diagnose the distributed I/O devices?
S7-300 CPU 31x -- Setting up and parameterizing hardware -- Initializing and parameterizing modules (GSD, Updates)
How can I prevent error 13:76 and 3311 when compiling the technology of a Technology CPU?
How do you have the web pages updated automatically in STEP 7 (TIA Portal) and how do you incorporate the user-defined web pages with relative path names?
Why must you never remove a memory card when the S7-300/S7-400/S7-1200/S7-1500 CPU is in operation (RUN)?
How do you configure the SIMATIC MV440 / MV420 code reader device with STEP 7 (TIA Portal) as a PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
How do you connect the SIMATIC Field PG to the bus system to parameterize and diagnose the distributed I/O devices?
How do you configure the SIMATIC MV440 code reading system as PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
How can time and date be acquired from a GPS signal?
How can you protect the S7-300/400 against unauthorized access from the LAN (local area network)?
What options exist for assigning passwords?
Master / Slave (SIMOVERT) communication on the DP PROFIBUS
What can you do if new modules, e.g. CPUs, are missing in the STEP 7 module catalog?
Where can I procure the GSD files for my S7-300 CPUs?
How do you configure time synchronization?
What is the startup behavior of an S7-300/400 CPU when you have configured an "empty" DP master system with "Startup when expected/actual configuration differ", but no slave is incorporated?
What are the conditions for assigning the addresses of I/O modules (central or distributed) to an S7 CPU?
How do you connect a SIMATIC S7-300 as DP slave to a Y link in the hardware configuration of STEP 7?
Machine Vision / Code reading systems -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Why can the HTML pages no longer be displayed in "Install" mode of the SIMATIC camera systems VS130, MV420 and MV440?
How do you connect an MV320 hand-held barcode reader to an ET 200S and ET 200SP?
How do you configure the SIMATIC MV440 / MV420 code reader device with STEP 7 (TIA Portal) as a PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
How do you perform a firmware update on an MV420/440?
How do you use Notepad++ to generate a match string message and transfer it with HyperTerminal?
Which hardware can be connected to the USB port of HMI operating devices?
How do you configure the SIMATIC MV440 code reading system as PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
How do you connect the MV440 sensor to an S7-300 controller using ASM456?
How do you connect a SIMATIC HawkEye 4x(T) handheld code reading system to an ET 200S?
What should you watch out for when using a stationary code reading system with a hand-held lens in the immediate vicinity of a laser system?
What options do you have for connecting a handheld He4xT to a PC and what should you pay attention to here?
How do you configure the SIMATIC MV440 code reading system as PROFINET IO device on the PROFINET IO system of a SIMATIC S7-300?
Part number:

Description
The documentation included in this entry describes how to connect a SIMATIC MV440 code reading system to a SIMATIC S7-300 via PROFINET IO.
In this example, a CPU319-3PN/DP is used as PROFINET IO controller.

The following figure illustrates this device configuration.


Fig. 01

Documentation
PROFINET_IO_with_MV440_en.pdf ( 1857 KB )

Sample programs
The "41726666_PROFINET_IO_with_MV440.zip" file provides the following sample programs and the components required as a download.

  • The STEP 7 project "MV440.zip" that includes the configuration of a CPU319-3PN/DP as PROFINET IO controller and a SIMATIC MV440 code reading system as PROFINET IO device. The sample program "Example.zip" is integrated in the STEP 7 application program of the CPU319-3PN/DP.
  • The sample program "Example.zip" that is on the CD included in the delivery package of the SIMATIC MV440 code reading system.
  • The GSD file of the SIMATIC MV440 code reading system, which is on the CD included in the delivery package of the SIMATIC MV440 code reading system.

PROFINE_IO_with_MV440.zip ( 841 KB )

 Entry ID:41726666   Date:2010-04-15