show the entry list
Industrial Ethernet S7-300/400 CPs -- Product information -- Determining performance and quantity frameworks
How many connections and communication jobs do SIMATIC S7-300 and S7-400 support simultaneously?
Which connection resources are occupied in the S7-300 CPU for communication connections and services of the Industrial Ethernet CP?
Which connection resources are occupied in the S7-400 CPU for communication connections and services of the Industrial Ethernet CP?
What are the system limits in an F CPU for safe bidirectional data communication using S7 Communication?
Where do you find information on transmission times on the PROFIBUS or Industrial Ethernet?
Increasing the CPU load for a data length of greater than 240 bytes in the case of Send/Receive communication with Industrial Ethernet CPs
What RAM capacity does the CP 343-1 IT make available for FTP services?
Why under certain circumstances are there very long response times with TCP connections?
PROFIBUS S7-300/400 CPs -- Product information -- Determining performance and quantity frameworks
How many connections and communication jobs do SIMATIC S7-300 and S7-400 support simultaneously?
Where do you find information on transmission times on the PROFIBUS or Industrial Ethernet?
Maximum number of CP 342-5 that can be operated simultaneously
S7-300 CPU 31x -- Product information -- Determining performance and quantity frameworks
How many connections and communication jobs do SIMATIC S7-300 and S7-400 support simultaneously?
Which connection resources are occupied in the S7-300 CPU for communication connections and services of the Industrial Ethernet CP?
What are the system limits in an F CPU for safe bidirectional data communication using S7 Communication?
How can you determine the size of the load memory and main memory of a SIMATIC S7-300/400 CPU?
What restrictions are there for active jobs when communicating with SFC 58 / SFC 59 and SFB 52 / SFB 53 via PROFIBUS DP and PROFINET IO?
Where do you find information on transmission times on the PROFIBUS or Industrial Ethernet?
What is a hardware interrupt and how do they work in the S7-300 system?
What is the maximum number of OPs that a CPU S7-300 can communicate with?
What can you do when the power requirement of the modules in the subrack exceeds the power supply provided by the CPU on the backplane bus?
Does PROFIBUS DP communication use connection resources?
What is the maximum number of CP modules that can be slotted in a SIMATIC S7-300/400 station?
Why, in the case of a networked SIMATIC S7, does the connection to the OP clear down when you call diagnostics functions with the PG or transfer blocks?
How many breakpoints can you insert when debugging a program?
S7-400 CPU 41x -- Product information -- Determining performance and quantity frameworks
How can you change the size of the available free main memory of a SIMATIC S7-400 CPU?
How many connections and communication jobs do SIMATIC S7-300 and S7-400 support simultaneously?
Which connection resources are occupied in the S7-400 CPU for communication connections and services of the Industrial Ethernet CP?
How many breakpoints can you insert when debugging a program?
What are the system limits in an F CPU for safe bidirectional data communication using S7 Communication?
How can you determine the size of the load memory and main memory of a SIMATIC S7-300/400 CPU?
Where do you find information on transmission times on the PROFIBUS or Industrial Ethernet?
What is a hardware interrupt and how do they work in the S7-400 system?
What restrictions are there for active jobs when communicating with SFC 58 / SFC 59 and SFB 52 / SFB 53 via PROFIBUS DP and PROFINET IO?
How many connections and communication jobs do SIMATIC S7-300 and S7-400 support simultaneously?
Part number:

Description
The maximum number of connections and communication jobs that an S7-300 or S7-400 supports depends on the CPU and CP used.
Each connection requires connection resources for the end point or for the transition point (e.g. CP) on the stations concerned. The number of connection resources is CPU/CP-specific. If all the connection resources of a communication partner are occupied, no new connection can be set up.

More information on the maximum number of connection resources is available in the Technical data of the S7-300 CPUs.

More information on the maximum number of connection resources is available in the Technical data of the S7-400 CPUs.

An overview of the services and quantity frameworks that the CPUs with integrated PN interface support is available in Entry ID: 18909487.

Information on which communication connections of the Industrial Ethernet CPs need connection resources of the CPU is available in Entry IDs: 42480411 and 42480718.

Information on the maximum permitted number of simultaneous connections via CP is available in the relevant CP manuals in the chapter entitled "Performance Data".

An overview of the services and quantity frameworks that the Industrial Ethernet CPs of S7-300 and S7-400 support is available in Entry IDs: 16767769 and 15368142.

 Entry ID:415725   Date:2010-05-17