show the entry list
Micromaster 4 -- Commissioning and operation -- Control via Terminal Blocks
MICROMASTER 4: Can I also use pushbuttons (without relay interconnection) to control my MICROMASTER?
MICROMASTER 4: Is it possible to switch-on the inverter via digital inputs and ON/OFF1 and switch-off the inverter via digital inputs and OFF2?
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): Can an analogue output be used as a digital output?
How can I suppress noise on measuring signals at the analog outputs of a drive inverter so that I can carry-out measurements using an oscilloscope?
MICROMASTER 4 (MM4): What parameters do I have to set on an MM440 to give the same binary fixed frequency selection functionality as 6SE32?
MICROMASTER 4 (MM4), SINAMICS G120: What is the difference between the control terminals for MM4 and SINAMICS G120?
Are the binary input command functions RUN right and RUN left the same on the MM4/SINAMICS G120 as on previous MICROMASTER products?
MICROMASTER 4 (MM4): How do I switch between two analogue inputs on MM440?
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): How can I parameterize a changeover between main and additional setpoint?
MICROMASTER 4 (MM4): How can I implement a center zero setpoint operation with the motor potentiometer?
MICROMASTER 420 (MM4): Is 3-wire control possible on the MM420?
MICROMASTER 420 (MM4): How do I set up the analogue input of the MM420 as a 4-20mA current loop?
MICROMASTER 4 (MM4), SINAMICS G120/G120D (CU2x0x): How can I switch between different ramp times?
Sinamics G120 -- Commissioning and operation -- Control via terminal block
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): How can I parameterize a changeover between main and additional setpoint?
SINAMICS G120 (CU 2x0x-2): Where do I find tips to the use of the motor holding brake and the reverse command?
SINAMICS G120 (CU2x0-2x): How can I configure my SINAMICS to keep running at the last valid speed reference received in the event of a loss of setpoint, when using PROFIBUS?
SINAMICS G120: How can I configure the Inverter to keep running at the last valid speed reference received in the event of a loss of setpoint or a wire breakage when using an analog 4 to 20mA reference signal?
SINAMICS G120 (CU2x0x): Rapid traverse / crawl changeover as shown in a conveyor application
After using macro 17 why can I no longer switch off my G120 / G120C?
Why can the main contactor of my SINAMICS G120 Power Module PM240 no longer be opened (de-energized)?
How can the MOP setpoint be tracked to another setpoint source with a SINAMICS G120 CU (from V3.0)?
For the CU2xy-2 of the SINAMICS G120 with firmware version V4.4, how can the analog inputs be parameterized für 4…20mA with monitoring?
Is it permissible to connect safety limit switches with magnetically-operated reed contacts to fail-safe SINAMICS G120 digital inputs?
SINAMICS G120: Information on using a 230V switching voltage at the relay outputs DO 0 and DO 2 of the CU230P-2.
MICROMASTER 4: Can I also use pushbuttons (without relay interconnection) to control my MICROMASTER?
MICROMASTER 4: Is it possible to switch-on the inverter via digital inputs and ON/OFF1 and switch-off the inverter via digital inputs and OFF2?
What is the impedance on the analogue input of the G120?
MICROMASTER 4 (MM4), SINAMICS G120/G120D (CU2x0x): How can I switch between different ramp times?
MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): Can an analogue output be used as a digital output?
Is it possible to parameterize the digital inputs of the SINAMICS G120 CU240E for NPN and PNP logic?
How do I re-parameterize analog output 0 of my G120 from 0-20mA to 0-10V? How do I correctly scale analog output 0 of my G120?
How can I suppress noise on measuring signals at the analog outputs of a drive inverter so that I can carry-out measurements using an oscilloscope?
MICROMASTER 4 (MM4), SINAMICS G120: What is the difference between the control terminals for MM4 and SINAMICS G120?
Are the binary input command functions RUN right and RUN left the same on the MM4/SINAMICS G120 as on previous MICROMASTER products?
MICROMASTER 4: Can I also use pushbuttons (without relay interconnection) to control my MICROMASTER?
Part number:

Normally, MICROMASTER expects a steady-state ON / OFF command (switch). In order to control a MICROMASTER drive using a pushbutton (pulse/momentary contact signal), then generally a relay interconnection is required. However, for frequency inverters that have free function blocks (FFB), then these can also be used to control an inverter using pushbuttons.

As an example, the “ON / OFF 1” (P0840) is used in the following examples. However, there are additional options to realize the interconnection e.g. “ON/OFF 1 with reversing” (P0842) and “Reversing” (P1113), refer to the Parameter List and Function Manual.

  Exclusion:

  • This FAQ can be used for MICROMASTER 430, 440 and SINAMICS G120 with CU240x FW < V4.0.
  • Only a limited number of FFB are available.

 

The following parameter assignments should be made for the examples:

Example 1: ON/OFF 1 using one NO contact and one NC contact, 2 digital inputs
Parameter Description Setting Description Notice
P0700 Selection of command source 2 Terminal Default setting
P0701 Function of digital input 1 99 Enable BICO parameterization ON via push-button, NO
P0702 Function of digital input 2 99 Enable BICO parameterization OFF via push-button, NC
P0840 ON/OFF1 command source using BICO r2841 output of RS-Flip-Flop 1 ON-signal via RS-FF- output
P2800 Enable FFB 1 Enable FFB Free function blocks
P2801.09 Activate FFB 1 Enable NOT 1  
P2801.14 Activate FFB 1 Enable RS-FF 1  
P2828 defines input of NOT 1 element r722.1 status of digital inputs OFF-Signal connected to NOT-input
P2840.0 define inputs of RS-Flip-Flop 1 r722.0 status of digital inputs ON-Signal connected to RS-FF-input
P2840.1 define inputs of RS-Flip-Flop 1 r2829 Output of NOT 1 element Negated OFF-Signal connected to RS-FF- input

 

Example 2: ON/OFF 1 using two NO contacts, 2 digital inputs
Parameter Description Setting Description Notice
P0700 Selection of command source 2 Terminal Default setting
P0701 Function of digital input 1 99 Enable BICO parameterization ON via push-button, NO
P0702 Function of digital input 2 99 Enable BICO parameterization OFF via push-button, NC
P0840 ON/OFF1 command source using BICO r2841 output of RS-Flip-Flop 1 ON-signal via RS-FF- output
P2800 Enable FFB 1 Enable FFB Free function blocks
P2801.14 Activate FFB 1 Enable RS-FF 1  
P2840.0 define inputs of RS-Flip-Flop 1 r722.0 status of digital inputs ON-Signal connected to RS-FF-input
P2840.1 define inputs of RS-Flip-Flop 1 r2829 Output of NOT 1 element OFF-Signal connected to RS-FF- input

 

Example 3: ON/OFF 1 using one NO contact, 1 digital input
Parameter Description Setting Description Notice
P0701 Function of digital input 1 99 Enable BICO parameterization ON-/OFF-signal via DIN1
P0840 ON/OFF1 command source using BICO r2841 output of RS-Flip-Flop 1 ON-signal via RS-FF- output
P2800 Enable FFB 1 Enable FFB Free function blocks
P2801.00 Enable FFB 2 AND 1 Enable  
P2801.01 Enable FFB 2 AND 2 Enable  
P2801.14 Enable FFB 1 RS-FF 1 Enable  
P2802.00 Enable FFB 1 Timer 1 Enable  
P2810.00 AND 1; input A r2852 Timer 1 output  
P2810.01 AND 1; input B r2842 RS-FlipFlop 1 Not-output  
P2812.00 AND 2; input A r2852 Timer 1 output  
P2812.01 AND 2; input B r2841 RS-FlipFlop 1 output  
P2840.00 Inputs of RS-FlipFlop 1 r2811 AND 1 output  
P2840.01 Inputs of RS-FlipFlop 1 r2813 AND 2 output  
P2849 Input signal of timer 1 r0722.0 Binary input values Switch-on/switch-off via DIN1
P2850 Delay time of timer 1 0.0 Factory setting Plant/system dependent
P2851 Mode timer 1 3 Pulse generator [Sec]

 

 Entry ID:41158384   Date:2010-02-10 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour