Description With the S7 program available for download in this FAQ document you can acquire the UTC time and date information from a GPS signal. This is effected with the help of a GPS mouse which receives the GPS signal in the form of an NMEA protocol and transmits it to a
SIMATIC S7-300/400 CPU for further processing.
The current time and date information is used to set the CPU module clock.
40929072_GPS_Data_Time_en.pdf ( 377 KB )
40929072_GPS_Data_Time.zip ( 419 KB )
Creation environment The pictures and downloads in this FAQ document have been created with STEP 7 V5.4 + SP5.
Keywords RMC sentence, system clock
|