|
Question: With which safety integrity according to IEC 62061 and ISO 13849-1 can a combination of a power contactor and a circuit-breaker (with undervoltage release) be assessed in a safety function?
Answer: Max. SIL 2 according to IEC 62061 or PL d in accordance with ISO 13849-1 can be achieved in conjunction with a safety-related evaluation, for instance a fail-safe controller or a safety relay.
The attached document explains the entire issue in details.
40349715_FAQ_functional_safety_circuit_breaker_en.pdf ( 571 KB )
Attachments::
ZIP file including following four files:
- Project file for the Modulare Safety System MSS
- SET project file in german
- SET project file in english
- Informations regarding mirror contacts
FAQ_40349715.zip ( 543 KB )
Search items:
NOT-HALT NOT-AUS E-STOP EMERGENCY-STOP EMERGENCY-Shut-Down Netztrenneinrichtung spannungsfreischalten Stillsetzen shutdown im Notfall Sicherheitskategorie safety category Redundanz redundancy SET Sistema safety reliability Zuverlässigkeit Ausfallrate failure rates MTTF_d MTTFd MTBF FIT B10 Percenteage Percentage Ratio of dangerous failures faults Anteil gefahrbringender Ausfälle SIL PL KAT
|