show the entry list
Mobile Panels -- Product information -- Determining performance and quantity frameworks
What are the functional differences between the different SIMATIC panels?
Which HMI components can you connect with S7-200 CPU and what should you watch out for when doing so?
Why do you get a warning when generating the block FB163, F_FB_RNG_16 and why cannot you load the block when using the Mobile Panel 277F IWLAN and an S7 CPU 315F (with PROFINET)?
What support does Siemens AG offer to make products comply with FDA regulations?
F Technology CPU 300/400 -- Creating and editing F programs -- Creating and editing F programs
How do you read out signals which cause a TRIP from an S7-400F/FH and log them on the Operator Station (OS)?
Why do you get a warning when generating the block FB163, F_FB_RNG_16 and why cannot you load the block when using the Mobile Panel 277F IWLAN and an S7 CPU 315F (with PROFINET)?
Which programming languages are available for programming a fail-safe controller?
Why does the load CFC update procedure abort with the error message: "Load procedure aborted"?
Why can't you load fail-safe blocks into the CPU?
F library
Distributed Safety V5.2 SP1 - Note on Saving in the LAD/FBD Editor if the F-Global DB is Missing
Why do you get a warning when generating the block FB163, F_FB_RNG_16 and why cannot you load the block when using the Mobile Panel 277F IWLAN and an S7 CPU 315F (with PROFINET)?
Part number:

The FB163, F_FB_RNG_16 cannot be used for the PROFINET CPUs listed below. It exceeds the maximum permissible block size. The following warning is issued when the block is generated:
"The F block FB163 or the associated automatically generated F block exceeds the maximum size supported by the F CPU configured."

You can only use the FB162, F_FB_RNG_4 with S7 PROFINET CPUs 315F and the following order numbers. Up to four Mobile Panels 277F IWLAN can be used it.

  • 6ES7315-2FH10-0AB0, CPU315F-2 PN/DP, 192KB
  • 6ES7315-2FH13-0AB0, CPU315F-2 PN/DP, 256 KB

Keywords:
Effective range

 Entry ID:40347347   Date:2010-01-13 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour