show the entry list
Microbox -- Setting up systems -- Installing and upgrading software
Compatibility Tool for Automation and Drive Technology
What is the compatibility of SIMATIC Rack PCs, Box PCs and Panel PCs?
Which SQL database can you use for archiving tags and messages with WinCC flexible Runtime on an Industrial PC?
How do you install a WinCC flexible Runtime on a Microsoft Windows XP embedded operating system?
What should you watch out for when using the Enhanced Write Filters (EWF) on SIMATIC IPCs with Windows XP Embedded Standard?
Why does the installation of SQL Express 2005 on a SIMATIC IPC with embedded operating system abort?
Box PC -- Setting up systems -- Installing and upgrading software
Which SQL database can you use for archiving tags and messages with WinCC flexible Runtime on an Industrial PC?
How do you install a WinCC flexible Runtime on a Microsoft Windows XP embedded operating system?
What should you watch out for when using the Enhanced Write Filters (EWF) on SIMATIC IPCs with Windows XP Embedded Standard?
How can you install RMOS using 2 GB SIMATIC PC USB FlashDrives?
Why does the installation of WinAC RTX 2005 (SP1) and of WinAC RTX 2008 abort?
Why does the software installation fail even though the memory card (Compact Flash Card) of the SIMATIC PC (without hard disk) indicates sufficient space?
Panel PC -- Setting up the system -- Installing and upgrading software
Which SQL database can you use for archiving tags and messages with WinCC flexible Runtime on an Industrial PC?
How do you install a WinCC flexible Runtime on a Microsoft Windows XP embedded operating system?
What should you watch out for when using the Enhanced Write Filters (EWF) on SIMATIC IPCs with Windows XP Embedded Standard?
What should you watch out for when installing the Service Pack 1 of Windows Vista on a SIMATIC Panel PC 677B with pushbutton front?
Why does the software installation fail even though the memory card (Compact Flash Card) of the SIMATIC PC (without hard disk) indicates sufficient space?
Why does the installation of WinAC RTX 2005 (SP1) and of WinAC RTX 2008 abort?
What should you watch out for when using the Enhanced Write Filters (EWF) on SIMATIC IPCs with Windows XP Embedded Standard?
Part number:

Description:
You wish to install software or update software in a system protected by EWF mode (Windows XP Embedded Standard). If you disable the EWF for drive C:\ using the command "ewfmgr c: -commitanddisable" without rebooting the system beforehand, in rare cases it might happen that the system no longer starts after rebooting. The following message is displayed:

"Windows could not start because the following file is missing or corrupt:
WINDOWS\SYSTEM32\CONFIG\SYSTEM..."

Cause:
The Windows Embedded Standard 2009 Installation on SIMATIC IPCs used a customized Registry entry. This Registry entry leads to the behavior described.

Remedy:
Install the attached Registry patch in order to be able to change the Registry entry. Installing the "REGFILTER_Patch.reg" Registry patch changes the Windows Registry.

Proceed as follows to install in a system protected by EWF Mode.

Instructions:
 
No. Procedure:
1 Reboot the system.
2 Open the Windows input prompt "Start > Run...", enter the command "cmd" and then <ENTER>.
3 Switch off the EWF by entering the command "ewfmgr c: -commitanddisable" and then <ENTER>.
4 Quit the input prompt by entering "exit" and then <ENTER>.
5 Reboot the system.
6 Copy the "REGFILTER.zip" file into a directory on your computer and unpack the file.
7 Double-click the "REGFILTER_Patch.reg" Registry patch to execute it.
8 Switch on the EWF again with the command "ewfmgr c: -enable".
9 Reboot the system.

Download:
Below is the Registry patch for downloading.

Regfilter.zip ( 245 bytes )

 Entry ID:40108744   Date:2011-09-14 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour