Description: In the preinstallation of the bundle HMI IPC 477C with WinCC V7.0 SP1, the German version of Microsoft SQL Server Management Studio Express Service Pack 2 (SSMSE SP2) was installed.
There are familiar mechanisms you can use to change the language (German and English) of the Windows XP embedded operating system and WinCC. If you wish to work directly in the SQL database, the "SSMSE SP2" is only available in German.
If you need the "SSMSE SP2" in English, you can uninstall the German version and install the English version. You can procure the English version free of charge from the following Microsoft link: "Microsoft SQL Server Management Studio Express" .
Download the SQLServer2005_SSMSEE.msi file and not the SQLServer2005_SSMSEE_x64.msi file.
Instructions:
| No. |
Procedure |
| 1 |
Uninstall the German version of Microsoft SQL Server Management Studio Express on your IPC 477C under "Start > Settings > Control Panel > Software". |
| 2 |
Install the English version of Microsoft SQL Server Management Studio Express that you have procured from the link specified above. |
|