show the entry list
WinCC flexible ES -- Working with projects -- Creating, editing, archiving and copying projects
What do you have to do if you can no longer access symbols and data blocks of STEP 7 from an integrated WinCC flexible project?
Which entries are available on the internet for migration to STEP 7 (TIA Portal) and WinCC (TIA Portal)?
How can you change the column width of picture objects in WinCC flexible?
In WinCC flexible, how can you prevent pictures and picture objects being fitted automatically when you change the screen resolution (possibly widescreen)?
How do you activate access protection for a STEP 7 project and set up a user as project editor?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
What are the solutions offered for working with different versions of WinCC flexible?
Which problems might arise if the "log.LDF" file is not available in a WinCC flexible project?
Why does WinCC flexible close again automatically after the program start?
How do you save WinCC flexible projects / libraries in the format of an earlier version of WinCC flexible?
How can you delete unused tags or objects from a WinCC flexible project?
What options do you have for copying pictures from one WinCC flexible project to another?
Copying HMI projects integrated in SIMATIC STEP 7 at file level
How can you open a WinCC project integrated in STEP 7 faster?
How do you archive projects in WinCC flexible and which files are required?
How do you back transfer the projects of an operator panel and what should you watch out for?
Which connector cables are available for connecting to SIMATIC Panels?
WinCC flexible ES -- Configuring and programming communication -- Configuring communication to S7
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
How can you visualize the current status of the CPU on a WinCC flexible operator panel?
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?
How do you use WinCC flexible to configure communication between an operator panel and an S7 station via S7 routing?
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options?
Which ports are used by WinCC flexible?
How can you increase the performance of HMI devices?
Which settings do you need to make to access a panel and an S7-200 controller via TeleService?
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet?
How do you configure a PROFINET connection to an S7 controller in WinCC flexible?
How do you specify the MPI address of an FM in the HMI configuration tool if the address doesn't appear in the HW Config and is thus unknown?
How do you connect a panel to a SIMATIC H station?
What settings have to be made for a PROFIBUS DP connection between a panel or a PC with WinCC flexible Runtime and an S7-200?
Why is the communication driver marked "orange" in WinCC flexible when another Ethernet communication is added to an existing MPI/DP?
PROFIBUS communications between Windows-based operator panel (configured with WinCC flexible 2004) and WinAC Basis / WinAC RTX V4.0
How do you configure communication between the WinCC flexible Runtime and WinLC via SOFTBUS on a PC?
How do you configure communication between WinCC flexible Runtime or a Windows-based operator panel and an S7-200 (CP 243-1) via Ethernet?
STEP 7 -- Working with projects -- Creating and editing projects
How do you compare blocks in a multiproject?
What are the requirements for migrating a STEP 7 V5.x project to STEP 7 Professional (TIA Portal)?
How do you link a self-made online help to a programmed block in STEP 7 V5.x?
How do you display the diagnostics buffer of a SIMATIC CPU with integrated web server on a SIMATIC Panel?
How do you install the improved block protection for FBs and FCs in STEP 7 V5.5 onwards?
In STEP 7, why can the "Find/Replace" dialog not be displayed in the LAD/STL/FBD editor?
How do you integrate a WinCC flexible project in STEP 7?
How can you improve the performance in the SIMATIC Manager and in the STEP 7 project?
Why can you no longer choose the options (Display, Filter, Generate, Delete) in the menu item "Tools > Reference data >"?
How do you save a STEP 7 project as read-protected on an MMC in an S7-300 CPU?
How do you activate access protection for a STEP 7 project and set up a user as project editor?
How do you update the STEP 7 hardware catalog in STEP 7 V5.2 onwards?
How can you load projects to a memory card and back again to a PG/PC?
Information about "Loading and testing programs"
How do you integrate an existing WinCC project into a STEP 7 project?
What are the advantages of the "Multiproject" function for large networked projects?
What is the significance of the initial and actual values of a data block?
Why can projects, blocks or the HW Config either not be opened at all or only opened with error messages or only as "read only"?
How do you integrate a WinCC flexible project in STEP 7?
Part number:

Description
The following points are described below:

  1. Integration of a WinCC flexible project in STEP 7.
  2. Possible causes of error when it is not possible to integrate a WinCC flexible project in STEP 7.

Instructions
 
No. Integration of a WinCC flexible project in STEP 7
1

Proceed as follows to integrate a WinCC flexible project in STEP 7.

  1. Open the WinCC flexible configuration.
  2. Select the menu command "Project > Integrate in STEP 7...".
    The "Integrate in STEP 7 projects" dialog opens.
  3. Select the relevant STEP 7 project in the dialog box.
    If the project you desire is not listed, navigate via the search field to the folder in which the STEP 7 project is located.
    Integration is executed once you select the STEP 7 project.


Fig. 01

Note
The STEP 7 project does not have to be open for this.

2

Parameterization of the connection / communication partner
In the "Stand alone" mode you have set all the connection parameters to the controller manually.
In the "Integration" mode you can define the station via which the communication partner is to be addressed using the selection menu. The addresses are then transferred automatically.
Furthermore, using this measure with the tags, you can access the symbolic connection.

  1. Open the STEP 7 project in which you previously integrated the WinCC flexible project.
  2. Mark the HMI station and double-click to open the "Configuration" of the HMI station.
  3. Open the "Properties" of the operator panel's interface and define the interface and address.


Fig. 02

  1. Switch to the WinCC flexible configuration and open the "Connections" in the project tree via "Communication > Connections".
  2. Select the relevant station under the "Station".
    The "Partner" and all the other parameters are transferred automatically.

This completes integration of the WinCC flexible project.

Possible causes of error when it is not possible to integrate a WinCC flexible project in STEP 7.

If the function for integrating the WinCC flexible project is grayed out or not available, this might be due to the following reasons.

  • You must install WinCC flexible Integration, because WinCC flexible was installed before STEP 7.

    Instructions
  1. Via the Control Panel you call the WinCC flexible Setup and change the installation.
    Control Panel/Software/SIMATIC WinCC flexible  Button: Change/Delete
  2. Activate the integration of STEP 7.
    The "WinCC flexible Integration" and "STEP 7" check boxes must be checked.
    (You need the WinCC flexible installation CD for this.)

Note
If you install the STEP 7 software before installing WinCC flexible, the WinCC installation routine recognizes the installation of STEP 7 and automatically installs support for integration in STEP 7.
If making a custom installation of WinCC flexible, make sure to activate the option "Integration in STEP 7".

  • If STEP 7 is already installed and you make an update for STEP 7, e.g. by installing a Service Pack, then you have to reinstall STEP 7 Integration in WinCC flexible.

    Instructions
  1. Via the Control Panel you call the WinCC flexible Setup and change the installation.
  2. Deactivate the integration of STEP 7.
  3. Then restart the Setup and activate the integration of STEP 7.
    (You need the WinCC flexible installation CD for this.)

You cannot integrate Micro Panels, e.g. a TP177micro, into STEP 7.

 Entry ID:38797080   Date:2010-01-29