show the entry list
WinCC -- Setting up development environments -- Installing / setting up operating systems
Why do other WinCC stations not appear in the network environment on the Windows 7 and Windows Server 2008 PCs?
Why should you not install the Microsoft security patches KB2467174, KB2467175, KB2465361 and KB2465367 in WinCC, PCS 7 and WinCC Professional V11?
What should you watch out for when using WinCC in a domain?
Which Microsoft Patches ("Security Patches" and "Critical Patches") have been tested for compatibility with SIMATIC WinCC?
What should you pay attention to when using WinCC with OEM operating systems?
How do you uninstall SP3 of Microsoft Windows XP?
Detailed information via the installed version of Microsoft Windows
Why can the WinCC uniclient not open the project from the server?
What restrictions are there for assigning the computer name for WinCC?
Logging off USB sticks from the operating system
How can you prevent Microsoft Windows Explorer from being opened as soon as you connect a USB stick to the computer or insert a CD/DVD in a drive?
How can you prevent the "Autoplay" function when inserting a CD/DVD or when connecting a USB device?
What should you pay attention to when using WinCC with OEM operating systems?
Part number:

Description:
It is not recommended to install WinCC on OEM operating systems of third-party PC manufacturers. The OEM operating systems can be adapted by the PC manufacturer concerned. In the case of WinCC, important parts of the Windows operating system might be missing.

We recommend using a Siemens Industrial PC with full operating system. More information on Siemens Industrial PCs is available at the following link:
http://www.siemens.com/Industrial-PC/

 Entry ID:38701636   Date:2009-10-06 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour