show the entry list
WinCC -- Configuring alarms and messages -- Displaying alarms and messages using Alarm Control
How can you import select messages in WinCC Alarm Control?
Why are spaces displayed at the beginning of the process-associated value (text) and characters truncated at the end?
How can you change the colors of the messages displayed in WinCC Alarm Control, also at Runtime, independently of the Alarm Logging settings?
How can you select messages in WinCC Alarm Control?
What are the differences in WinCC between message processing in the message list and in the archives?
Why does a limit message in WinCC remain although the value is once again within the configured limits?
How can I display the last message in the first line of the AlarmOCX?
What do you do if alarms are not displayed at Runtime?
How can you have multiline message texts displayed in Alarm Control?
How are messages shown in WinCC Alarm Control?
How can you have the logged-on user and computer name displayed in the alarm list in WinCC?
How do you use the "MsgFilterSQL" property of the WinCC Alarm Control in order employ an SQL statement to filter the messages to be displayed?
How can you have only selected messages displayed in the WinCC Alarm Control at Runtime?
How do you use the standard function "AXC_SetFilter()"?
What is the structure of the format instruction for displaying the contents of WinCC tag values at Runtime in the user text blocks of a message?
How can you filter messages in WinCC Alarm Control according to servers?
How do you display or print the content of the comments dialog box (comment, computer, author)?
Why are the column headers in the WinCC Alarm Control shown with the character string at runtime?
How can you change the column width of the message blocks with the mouse in WinCC Alarm Control when configuring in the Graphics Designer or in Runtime?
Why are only 1000 messages shown in the archive window although there are more in the archive?
What do the settings in "Apply project settings" in the Message Blocks tab mean when you configure the WinCC Alarm Control?
OS - WinCC -- Configuring alarms and messages -- Displaying messages using Alarm Control
How can you select messages in WinCC Alarm Control?
What should you do if there is no indication of origin in the message for redundant OS servers?
Text length of the 'Origin' message text in Alarm Logging
Determining the number of messages in WinCC
How are messages shown in WinCC Alarm Control?
Sorting the message lists in PCS 7 V5.x and V6
How can you have only selected messages displayed in the WinCC Alarm Control at Runtime?
How do you use the standard function "AXC_SetFilter()"?
How can you filter messages in WinCC Alarm Control according to servers?
What do the settings in "Apply project settings" in the Message Blocks tab mean when you configure the WinCC Alarm Control?
How do you display or print the content of the comments dialog box (comment, computer, author)?
How can you select messages in WinCC Alarm Control?
Part number:

Description:
The new WinCC Alarm Control provides you with the extensive option of selecting messages in Alarm Control during configuration and at Runtime. A detailed description is available in the WinCC Information System in the path: Working with WinCC > Setting up a Message System > Display of Messages during Runtime > Operation during Runtime > How to select messages.

Note:
If you enter a selection with several criteria, these criteria are linked as in an "AND" operation. You can link multiple selections as in an "OR" operation. You can create these selections both during configuration and during Runtime.

Example:
If you enter the criteria "Number less than 100" and "Number greater than 1000" in a selection, no messages are displayed, because this creates the SQL statement "MSGNR < 100 and MSGNR > 1000".

If you create a selection with the criteria "Number less than 100" and a selection with the criteria "Number greater than 1000" and you link these two selections, you get a display of all the messages numbered 1 to 99 and all the messages with numbers greater than 1000. The SQL statement created would be "MSGNR < 100 or MSGNR> 1000".

Instructions for creating selections during configuration:
 
No. Procedure
1 Add a WinCC Alarm Control (not WinCC Alarm Control (Classic) in the Graphics Designer. Open the Properties dialog of the WinCC Alarm Control and select the "Message lists" tab. Select "Selections > Edit...".


Fig. 01

2 Select "New..." to create your desired selection criteria.
3 No messages are displayed with this setting.


Fig. 02

4 With this setting, all the messages numbered 1 to 99 and all the messages with a number greater than 1000 are displayed.


Fig. 03


Fig. 04


Fig. 05

With these settings and links, all the messages numbered 1 to 99 and all the messages with a number greater than 1000 are displayed.

 Entry ID:38525996   Date:2009-09-16