show the entry list
ES - SIMATIC Manager -- Working with projects -- Compiling OS and loading OS
What should you watch out for when downloading from the WinCC/PCS 7 Engineering Station to the Operator Station (ES-OS download)?
Why aren't all the block icons updated during OS compilation?
Which settings should you check if OS loading fails with PCS 7 or the OS project cannot be activated?
Problems when mapping data blocks with the same name
How can you clear the following error message during OS compilation: "The number of parameters for the structured DM variables xxx of type yyy does not match the number of operator-controlled connections...".
What is the meaning of the error message "A structure conflict occurred when creating the structured DM variable XXXX of type YYYY..." when compiling the OS?
How do you set the TCP/IP protocol for PLC-OS data transfer?
What is the meaning of the warning in the log file "*** Warning(s) ***: The structure type XXXX has been changed since the last compilation. All associated structured tags (even other S7 programs) will be deleted on the OS." ?
How do you use the template pictures "@PCS7Typicals*.pdl" to create block icons?
What does the compile OS error message "302:3018 - There are process variables whose names are not unique within the project after replacing special characters..." mean?
Which messages may appear in the "Download OS" dialog box?
Why appears the error message "The number of external DM variables in WinCC exceeds the permitted in total number", although the necessary license is available?
With PCS 7, why can't you open the OS project on the OS after it is downloaded from the ES?
Which special characters/separators may not be used in PCS7 V4, V5, and how are they replaced during AS/OS transfer?
What are the requirements for performing an online delta loading of the OS?
Why does the automatic package update of the clients sometimes not work in case of a changes-only download?
What do you do if a text which is configured in the CFC appears different in runtime?
How is a text, which has been configured in the CFC, transferred into the OS during OS compilation, and what do you have to watch out for in particular during configuration?
Which work steps are necessary for a project update of a redundant server couple and the MultiClients in SIMATIC PCS 7 V5.x?
Which work steps are necessary for the update of the OS Runtime data for the migration from PCS 7 V5.x to SIMATIC PCS 7 V6.x?
What do you do in PCS 7 V7.0 if the OS compile process is interrupted because the WinCC project cannot be opened?
Why can WinCC tags have the status "write-protected" and thus cannot be edited, deleted or moved?
What has to be watched out for during the compilation of a modification into the OS-Station after the interface modification of a Function block?
Why can't you transfer the elements of an S7 structure or UDT to WinCC through OS compilation?
Why doesn't OS delta load from the SIMATIC PCS 7 ES work despite Runtime being active on the OS station?
Why do you get a warning to the effect that your OS project is running in demo mode when testing it on your ES?
How can you clear the error message "Download (310:88)"?
How can you correct the error message "OS is currently being loaded from another ES"?
How is server data (server package) generated and loaded?
After reloading the OS project to the server from the ES, how do you clear the undefined error message and the abort?
When compiling the OS project, how can you clear the internal error 15500 in the transfer.log file?
Why does the error message "FileCopyError ....WinCC6.0_Project\GraCS\Default.pdd" occur when making a delta load and what is the "Default.pdd" file for?
Why are texts no longer updated with PCS 7 V6.0 SP3 + SP3 Postfixes after an OS delta compilation and OS delta load?
How do you clear the error message "*** Error(s) ***: Error while requesting messages from the STEP 7 message server...."?
How do you clear the error message "Internal error: transfer of process variables has been aborted. Error number: 15424" when compiling the OS project?
How can you clear the error message "No DM variable can be created for a symbol without a name" during OS compilation?
Why can't you load a project via a network?
OS - WinCC -- Operation and maintenance -- Diagnosing errors
Why do you get the license error message "YMAINR9999 missing" although you are using only the license-free basic diagnostics?
How do you perform comprehensive diagnostics in PCS 7 and WinCC plants?
How can you back up the data of the Windows event viewer?
How do you install the User Mode Process Dumper for diagnostics with WinCC and PCS 7?
Which details does Technical Support need regarding inquiries on SIMATIC PCS 7?
Why are the DCOM settings of the WinCC OPC server reset after activating the OS Runtime?
Why is the message "Network not ready yet." displayed when an AutoStart is configured on the OS?
Why are the STEP 7 ActiveX controls (OCX) not shown on the OS server and OS client?
Why aren't all the block icons updated during OS compilation?
What are the causes of PCS 7 control technology and system messages and what measures are to be taken to clear them?
Why does the OS Login Box disappear sometimes in the background?
Length of mapped message texts
What should I do if the Split Screen Wizard closes with an error message?
Why do I get an error message when calling the loop display of a faceplate?
What is the meaning of the WinCC messages "PLC fault synchronous" and "PLC fault asynchronous"?
Why does it take 3 to 5 minutes for the Login Box to open on the client or until the message "No authorization for operation" is displayed?
What might be the cause that the hierarchy display in the overview area of the SIMATIC PCS 7 OS does not work?
Error Message "Group display: Tag .Eventstate does not exist"
Why does "?????" appear as a text on the range selector buttons in the overview area in OS runtime even though the text is available in the SIMATIC Manager?
Why does the error message 10111001 "The group display hierarchy has not been updated" appear?
Why aren't all the block icons updated during OS compilation?
Part number:

Description:
You have complete OS compilation without errors and warnings. During the course of this, the "Create/Update Block Icons..." function was also executed implicitly. Nevertheless, not all the block icons were updated. One reason for this might be that you are using more than 10 template pictures.

Instructions:
Limit your template pictures to a maximum of 10.
More information is available in the WinCC Information System in the path: Options > Options for Process Control > Graphic Object Update Wizard > Example: Creating object templates. A detailed description of how to use template pictures is available in Entry ID 26697820.

Keywords:
PCS7Typicals,  @PCS7Typicals, Faceplate

 Entry ID:38525786   Date:2009-09-16 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour