show the entry list
WinCC -- Product information -- System description
Which Details does Technical Support need regarding Inquiries on SIMATIC WinCC
Which user rights does a user have who belongs to multiple Windows user groups of which several are stored in the WinCC User Administrator?
Further information on the Catalog ST80 with regard to WinCC Communication
SIMATIC WinCC on PCs with AMD-Processors
How can you use the license for Microsoft SQL Server 2000 in conjunction with WinCC?
OS - WinCC -- Product information -- System description
Which user rights does a user have who belongs to multiple Windows user groups of which several are stored in the WinCC User Administrator?
How do you license archive tags in PCS 7 V7.0?
What is new about the license procedure for SIMATIC PCS 7 OS V6.0?
SIMATIC PCS 7 V6.x and V5.x in mixed mode on OS servers and OS clients
Which user rights does a user have who belongs to multiple Windows user groups of which several are stored in the WinCC User Administrator?
Part number:

Requirements:
You are using WinCC in combination with SIMATIC Logon.

Description:
An error has been discovered in the English WinCC documentation in the following path.
"WinCC Information System > Working with WinCC > Creating a User Administrator > WinCC Options for the User Administrator > SIMATIC Logon Option > Notes on Connecting WinCC/PCS7-OS"

As from WinCC V6.2 SP2, the behavior regarding which user rights a user has who belongs to multiple Windows user groups of which several are stored in the WinCC User Administrator is described incorrectly in the English documentation.

Rights of the logged-on user:
If the user belongs to one or multiple Windows user groups of which several are stored in the WinCC User Administrator, the rights of all these groups are assigned to that user.

 Entry ID:38487261   Date:2009-09-14 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour