show the entry list
ES - SIMATIC Manager -- Creating programs -- Using SFC
How do you reset error outputs without starting the productive sequencer?
How do you disable step time monitoring in the "Holding" mode?
What effect do the values "with" and "none" have in the "Enumeration" setting for setpoint values in SFC types and SFC instances?
What should you watch out for when using SFC charts/SFC type instances for delta loading, whose sequencers are processed in the "IDLE" state?
Why do you get the error message "Missing or invalid identifier" in the SCL compiler after upgrading from PCS 7 V6.1 to PCS 7 V7.0?
How can you change the message texts of an SFC chart in PCS 7?
What is the maximum number of transitions and alternative branches permissible in an SFC chart?
How do you make SFCs dynamic with Dynamic Wizard?
What should you watch out for when making online changes to the structure of an SFC types?
When do you use the Operation Type (EOP) technical function and when do you use the Function Type (EPH) technical function when defining your SFC type?
How do you use the "AUX_PRxx" inputs for message-associated values of an SFC instance?
How can you prevent the output LI_ERR being set on the SFC_CTRL block?
How can you start an SFC chart /SFC instance in the AUTO process mode by way of the block inputs?
How do you configure an operator request in an SFC type?
How do you proceed when there is a failure upon opening an SFC chart or SFC type in the SIMATIC Manager?
How do you optimize the size of the work memory for an SFC type?
How do you determine the size of the work memory which is occupied by an SFC type?
How do you leave one SFC sequencer and continue processing in another sequencer at a fixed target position?
How can you monitor an SFC type "online" (in test mode)?
What operating modes does the SFC have and what options are available for configuring sequencers?
How can you display the current operational status of a sequencer?
How can you display the operational display of a sequencer with a message of the SFC type instance?
How can pre- and afterprocessing be used in the sequence features of the SFC at SIMATIC PCS 7 V6?
When do I use a SFC-Chart and when a SFC-Type in SIMATIC PCS 7?
How do you visualize the current runtime of a step of an SFC sequence?
How do you configure an SFC type to ensure automatic interconnection of the block contacts?
How can you display the operational status of a sequencer with a message of a separate message-compatible block?
How can you resume a SFC sequence at the point of abortion upon restart of the CPU?
How do you switch an SFC chart into automatic mode?
What should you watch out for when doing a delta download of an SFC chart?
How do you expand user created blocks or standard blocks from the PCS 7 library so that they are listed in the Properties dialog of the SFC editor?
How do you make SFCs dynamic with Dynamic Wizard?
Part number:

Description
Proceed as follows to enter the Wizard Script:

  1. Open Explorer and double-click to start the file <...\Siemens\WinCC\Bin\DynWizEdit.exe>
    => DynWizEdit opens.
  2. In the dialog box below the menu bar set the required language.
  3. Open the menu <Dynamic Wizard> -> <Read Wizard Script>
    => The <Open> window opens with a list of all the available Wizard Scripts.
  4. Find the <SFCScript.wmf> file in the list and open it.
    => The Wizard Script is then entered and the message "0 Error(s), 0 Warnings" is displayed in the <Output window> window.
  5. This indicates that the Wizard Script has been successfully entered and compiled. Now close the DynWizEdit.

Making an SFC dynamic in the Graphics Designer:

  1. Open your image with the Graphics Designer, enter an OLE control from the object palette and select the type <SFC Control> from the <Insert OLE Control (OCX)> list. Acknowledge with <OK>.
  2. Open the Dynamic Wizard and click the (now newly available) tab <SFC>.
  3. Start the Wizard by double-clicking the Wizard Script <Configuring>.
  4. Run the Wizard and select the required SFC plan from the list and the display type <Overview or Excerpt>.
  5. Save your image and test the function in runtime.
 Entry ID:382599   Date:2010-10-29 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour