show the entry list
WinCC flexible ES -- Product information -- General information
What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook?
How do you make printouts on different printers in WinCC flexible PC Runtime?
How can you exchange data between USB storage devices on the Thin Client with an active RDP connection?
What are the functional differences between the different SIMATIC panels?
What options are there for creating a screenshot in WinCC flexible ES, WinCC flexible Runtime or on panels?
What support does Siemens AG offer to make products comply with FDA regulations?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
How do you send customer projects to Technical Support?
Why are PDF documents not displayed properly on the MP377?
Which GSD files are there for the Profibus DP operator panels?
Which GSDML files are there for the operator panels for Profinet IO?
Is there a Siemens contact for customer-specific software solutions, extensions to WinCC flexible or own applications for Windows CE Panels?
Multi Panel -- Creating HMI configurations -- Displaying and outputting documents
How can you use an operator panel to output a variable text input as barcode on a printer?
What options are there for creating a screenshot in WinCC flexible ES, WinCC flexible Runtime or on panels?
Why are PDF documents not displayed properly on the MP377?
How do you open a WORD document via an operator panel?
WinCC flexible RT -- Product information -- General information
Why does the "Lock program switching" function no longer work after upgrading from SIMATIC WinCC flexible Runtime 2008 SP2 to SP3?
What new features do Intel® Atom™ processors have and what advantages do SIMATIC IPCs with Intel® Atom™ processors offer when used with SIMATIC software?
Which licenses do you need to upgrade from WinCC flexible 2008 or WinCC V7 to WinCC V11 and in WinCC V11?
What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook?
How resistant to chemicals are the SIMATIC Panels and Panel PCs?
What options are there for creating a screenshot in WinCC flexible ES, WinCC flexible Runtime or on panels?
What support does Siemens AG offer to make products comply with FDA regulations?
What support does Siemens AG offer to make use of panels comply with FDA regulations?
What support does Siemens AG offer to make the use of WinCC flexible comply with FDA regulations?
What should you watch out with regard to licenses for WinCC flexible and panels?
How do you have csv archive files exported from WinCC flexible RT or a panel displayed graphically on the PC?
Which ports are used by WinCC flexible?
WinCC flexible Options -- Product information -- WinCC flexible /Sm@rtService (Teleservicing)
What options are there for creating a screenshot in WinCC flexible ES, WinCC flexible Runtime or on panels?
How do you have csv archive files exported from WinCC flexible RT or a panel displayed graphically on the PC?
How can you use a PC to simulate or realize sending e-mails in the case of an HMI station message?
What should you watch out with regard to licenses for WinCC flexible and panels?
What are the options for remote maintenance of a WinCC flexible Runtime system (Panel/PC) via the Internet (WAN)?
Connection to the SIMATIC WinCC flexible Sm@rtServer gets lost (with active screensaver or "Shut Down")
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
Why do you get the message "Under Construction" in WinCC flexible 2004/2005 when attempting to connect to the MiniWeb via the HTML viewer?
Why, when you call the Sm@rtClient, is only an empty page displayed in the Internet Explorer?
How do you send e-mails from a Windows CE panel or PC with SIMATIC WinCC flexible?
How do you send short messages (SMS) from an SIMATIC WinCC flexible HMI station to a mobile phone?
What options are there for creating a screenshot in WinCC flexible ES, WinCC flexible Runtime or on panels?
Part number:

Introduction:
Here, we describe how to create a screenshot in WinCC flexible ES, WinCC flexible RT and on panels.

Create screenshot with WinCC flexible ES / WinCC flexible RT
Create screenshot on a SIMATIC panel

Create screenshot with WinCC flexible ES / WinCC flexible RT
WinCC flexible permits printing of project documentation. Using the project documentation, you can make a screenshot of each screen configured.

Instructions:
Follow the instructions in the table below to create a screenshot of the configured screens in WinCC.
 
No. Procedure
1 Open the required WinCC flexible project.
2 Select the menu command "Project > Print project documentation..." (can also be selected with the key combination "Ctrl+P").
3 Select the "Content" tab and then activate the "Screens" option.
Create a preview of the log selected with the button marked in red in Fig. 01. A preview of the log is then created. The preview is for creating screenshots and formatting the data.


Fig. 01

4 Close all the windows.
5 A new folder ["Project_name"_(PRO_Documentation)] is created in the project directory. This folder contains a screenshot of each configured screen in "EMF" format.


Fig. 02

Note:
In WinCC flexible ES and WinCC flexible RT, you can also use the normal functions of your operating system to create a screenshot. In the "Windows" operating system you simply press the "Print" key to create a screenshot. It is stored in the Windows clipboard.

Create screenshot on a SIMATIC panel
There are two ways of creating screenshots on panels:

  • Connection via Sm@rtService
  • Using the CaptCE software

More information on the topic of remote access (Sm@rtService) to a panel is available in Entry ID: 19865167.
CaptCE software allows you to create a screenshot directly from the multi panel in the form of a bitmap file.

Warning:
The use of third-party software on multi panels has not been tested and approved. Therefore, we cannot give any guarantee that third-party software, such as CaptCE, will work properly. Please note, panels only support programs which are structured on MIPS/RISC or ARM architecture.

Hardware and software requirements:

  • MP 177 6" Touch, MP27x, MP37x or Mobile Panel 277
  • USB mouse for connecting to the MP (optional)
  • ProTool V6.0 SP2 or WinCC flexible
  • CaptCE from the following link: http://oohito.com/ under the keyword "Mobile Computer Software Gallery"
  • CF/MMC/SD card
  • Microsoft ActiveSync from V3.5 with a zero model cable only for MP270/370
    (for details of the cable assignment, refer to Entry ID: 29034071)
  • FTP download (see Entry ID: 26128938)

Installation of CaptCE on the multi panel

  • CaptCE software is available to download from the Internet at: http://oohito.com/mcsg/archives/category/wince

    Note:

    Depending on the version of your panel, you must follow the MIPS link for MP270/370 and the relevant ARM link for MP177/277/377.
    (Since this is a Japanese home page, it might be possible that not all the characters are displayed or you are prompted to install support of the font in the browser. The right menu bar is in English, so it is possible to navigate to the version of CaptCE appropriate for your panel.)
     
  • The CaptCE software comprises an .exe file named "CaptCE.exe". You simply have to transfer the "CaptCE.exe" file to the multi panel.
     
  • You can transfer the "CaptCE.exe" to the multi panel either with Microsoft Active Sync, only MP270 / MP370 (see Entry ID: 12933294) or with FTP download (see Entry ID: 26128938) or via a CF/MMC/SD card.
    Refer to the relevant manual to see which cards are permitted for your panel.
     
  • Create a new folder in the file manager for the multi panel and copy CaptCE.exe to that folder.


Fig. 03

  • Start the Control Panel and double-click on OP. Click the Save Registry and Save Files buttons in the Persistent Storage tab.

Creating screenshots as a bitmap file with CaptCE.exe in WinCE

  • Start the program by double-clicking on "CaptCE.exe". The program which is started is indicated in the taskbar by a "camera" icon.


Fig. 04

  • In order to create a current screenshot on the multi panel, double-click the "camera" icon. The current screen content is saved as a screenshot on the multi panel.
  • The screenshots which are created are saved directly under My Computer.


Fig. 05

  • You can transfer the screenshot to a PC either with Microsoft Active Sync (see Entry ID: 12933294) ) or via a CF card.
  • In order to close the program, press the ALT key (which is also possible on the screen keypad) and then click the camera icon on the taskbar.

Creating screenshots as a bitmap file from Runtime

  • To create a screenshot from Runtime, you can use the system function Program_start in ProTool or StartProgram in WinCC flexible in order to run "CaptCE.exe".
  • Configure a button or global key with the function Program_start or StartProgram and the parameter program name, e.g. \CaptCE\captce.exe.


Fig. 06

  • The "CaptCE" program is run the first time by simply pressing the key or clicking the button.
  • Every subsequent time you press the key or click the button, a screenshot of the current screen is created and saved on the multipanel under "My Computer".
  • You can transfer the screenshot to a PC either with Microsoft Active Sync (see Entry ID: 12933294) ) or via a CF card.
  • In order to close the program, switch to WinCE mode, press the ALT key (which is also possible on the screen keypad) and then click the camera icon on the taskbar.

Note:
Use the "PrintPicture" function to print a process image.

Keywords:
Screenshot, Hardcopy, 19724493

 Entry ID:38043669   Date:2009-09-03 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour