show the entry list
STEP 7 (TIA Portal) -- Setting up development environments -- Installing and upgrading software
How do you perform the firmware update V3.0 for the S7-1200 in STEP 7 (TIA Portal) by means of the web server?
Which license do you need to upgrade from STEP 7 version V5.x, V10.5 or V11 to the TIA Portal V12?
Which SIMATIC software can you install in 64-bit operating systems?
How can you install STEP 7 V11 in Windows XP with Turkish installed as Regional and Language option?
Why do you get a prompt to restart MS Windows after installing STEP 7 V11, although the PC has already been booted?
How do you update the hardware catalog in STEP 7 (TIA Portal)?
What are the requirements for installing STEP 7 (TIA Portal) V12?
Which devices and modules are supported by STEP 7 Professional V11 and WinCC Professional V11?
How can you install STEP 7 V11 in Windows XP with Turkish installed as Regional and Language option?
Part number:

Instructions
Installation of STEP 7 V11 might be aborted in Windows XP if the Regional and Language options are set to Turkish. The following error message is displayed:

  • An error occurred during setup .

Remedy
Change the Regional and Language options from Turkish to English or German. The procedure is described in the table below.
 
No. Procedure
1

Open the Control Panel in MS Windows by means of:

  • "Start > Control Panel" (Start menu in Windows XP), or
  • "Start > Settings > Control Panel" (classic Start menu as in earlier versions of Windows).
2

Open "Regional and Language Options" and select the "Regional Options" tab.


Fig. 01

3

In the drop-down list box under "Standards and formats", change the language from Turkish to English or German.


Fig. 02

4 Then click the "Apply" button, followed by "OK" to confirm.
5 You have to restart your PC to make the setting effective. Then you can install STEP 7 V11.
6 After installation you can change the Regional and Language options back to Turkish (as described in points 1 to 4).

Keywords
Change of language

 Entry ID:37855027   Date:2012-02-10 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour