show the entry list
OS - WinCC -- Operation and maintenance -- Diagnosing errors
Why do you get the license error message "YMAINR9999 missing" although you are using only the license-free basic diagnostics?
How do you perform comprehensive diagnostics in PCS 7 and WinCC plants?
How can you back up the data of the Windows event viewer?
How do you install the User Mode Process Dumper for diagnostics with WinCC and PCS 7?
Which details does Technical Support need regarding inquiries on SIMATIC PCS 7?
Why are the DCOM settings of the WinCC OPC server reset after activating the OS Runtime?
Why is the message "Network not ready yet." displayed when an AutoStart is configured on the OS?
Why are the STEP 7 ActiveX controls (OCX) not shown on the OS server and OS client?
Why aren't all the block icons updated during OS compilation?
What are the causes of PCS 7 control technology and system messages and what measures are to be taken to clear them?
Why does the OS Login Box disappear sometimes in the background?
Length of mapped message texts
What should I do if the Split Screen Wizard closes with an error message?
Why do I get an error message when calling the loop display of a faceplate?
What is the meaning of the WinCC messages "PLC fault synchronous" and "PLC fault asynchronous"?
Why does it take 3 to 5 minutes for the Login Box to open on the client or until the message "No authorization for operation" is displayed?
What might be the cause that the hierarchy display in the overview area of the SIMATIC PCS 7 OS does not work?
Error Message "Group display: Tag .Eventstate does not exist"
Why does "?????" appear as a text on the range selector buttons in the overview area in OS runtime even though the text is available in the SIMATIC Manager?
Why does the error message 10111001 "The group display hierarchy has not been updated" appear?
What are the causes of PCS 7 control technology and system messages and what measures are to be taken to clear them?
Part number:

Description:
The attached Excel file contains a list of control technology and system messages that might occur in the message system of the OS Runtime system. These messages are triggered not only by the PCS 7 Basic system, but also by PCS 7 Options (like SIMATIC BATCH and SIMATIC Maintenance Station).

As far as possible, we have defined one or more measures for each message, which should help you clear the messages and possibly avoid them in the future.

The Excel file is in German and English. You simply select the relevant button for the language you require. The "All" button displays both languages at the same time.

PCS 7 System message ( 2756 KB )

Note:
This list has been created from PCS 7 version V7.1 and the associated options. Most of the messages can also occur in previous versions. The measures specified should also apply there.

 Entry ID:37696303   Date:2011-03-01 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour