show the entry list
S7-300 CPU 31x -- Product information -- Determining performance and quantity frameworks
How many connections and communication jobs do SIMATIC S7-300 and S7-400 support simultaneously?
Which connection resources are occupied in the S7-300 CPU for communication connections and services of the Industrial Ethernet CP?
What are the system limits in an F CPU for safe bidirectional data communication via S7 Communication?
How can you determine the size of the load memory and main memory of a SIMATIC S7-300/400 CPU?
What restrictions are there for active jobs when communicating with SFC 58 / SFC 59 and SFB 52 / SFB 53 via PROFIBUS DP and PROFINET IO?
Where do you find information on transmission times on the PROFIBUS or Industrial Ethernet?
What is a hardware interrupt and how do they work in the S7-300 system?
What is the maximum number of OPs that a CPU S7-300 can communicate with?
What can you do when the power requirement of the modules in the subrack exceeds the power supply provided by the CPU on the backplane bus?
Does PROFIBUS DP communication use connection resources?
What is the maximum number of CP modules that can be slotted in a SIMATIC S7-300/400 station?
Why, in the case of a networked SIMATIC S7, does the connection to the OP clear down when you call diagnostics functions with the PG or transfer blocks?
How many breakpoints can you insert when debugging a program?
S7-400 CPU 41x -- Product information -- Determining performance and quantity frameworks
How can you change the size of the available free main memory of a SIMATIC S7-400 CPU?
How many connections and communication jobs do SIMATIC S7-300 and S7-400 support simultaneously?
Which connection resources are occupied in the S7-400 CPU for communication connections and services of the Industrial Ethernet CP?
How many breakpoints can you insert when debugging a program?
What are the system limits in an F CPU for safe bidirectional data communication via S7 Communication?
How can you determine the size of the load memory and main memory of a SIMATIC S7-300/400 CPU?
Where do you find information on transmission times on the PROFIBUS or Industrial Ethernet?
What is a hardware interrupt and how do they work in the S7-400 system?
What restrictions are there for active jobs when communicating with SFC 58 / SFC 59 and SFB 52 / SFB 53 via PROFIBUS DP and PROFINET IO?
How can you determine the size of the load memory and main memory of a SIMATIC S7-300/400 CPU?
Part number:

Description:
The example shown here explains how you can use your project to determine the size of the load memory and main memory in order to define the size of the memory cards needed, for example.

  1. Open the project and mark the block folder.
     
  2. Right-click and select "Object Properties".


    Fig. 01
     
  3.  In the new window you select the "Blocks" tab.


    Fig. 02
     
  4. You can also determine the size of the load memory by adding the user program and the system data (red marking),
    for example, 428 bytes + 710 bytes = 1138 bytes
    The memory card used in the S7 CPU must have this size at least.
     
  5. The required size of the CPU's main memory is displayed directly (yellow marking).

Keywords:
Memory size, MMC, MC

 Entry ID:36981866   Date:2009-08-06 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour