|
QUESTION:
How to evaluate a safety function by using SIMATIC S7 "standard output cards" switched off by the load voltage?
ANSWER:
ISO 13849-1
IEC 62061
Explanation for the application:
Following explanations attempt the possible evaluation of SIMATIC S7 standard output cards with IEC 62061 or ISO 13849-1.
The statements below do not contain any claim to completeness but should be a practical support in the comprehension and implementation of IEC 62061 or ISO 13849-1.
Attached you find a document which explains this issue detailled.
Anymore questions?
Please consult Technical Assistance of Low Voltage Switchgear via the mail adress or phone number shown in the header of the document.
IEC62061_ISO13849_Info_5_en.pdf ( 42 KB )
|