|
Description: IO devices that support the "Replace device without interchangeable medium" function can be replaced without the need for an interchangeable medium (Micro Memory Card, for example) with saved device name being slotted.
The replacement IO device no longer receives the device name from the interchangeable medium, but from the IO controller.
For this, the IO controller and the neighboring PROFINET devices of the replaced IO device must also support the "Replace device without interchangeable medium" function.
The IO controller uses the topology configured in STEP 7 to assign the device name and the neighbor relationships of the IO devices.
The IO controllers below support the "Replace device without interchangeable medium" function:
36752540_PROFINET_IO_Controller_list_en.pdf ( 19 KB )
The following IO devices support the "Replace device without interchangeable medium" function:
36752540_PROFINET_IO_Device_list_en.pdf ( 17 KB )
|