show the entry list
PROFINET general -- Product information -- System description
In the TIA Portal, how do you do a firmware update of the distributed IO?
Where can you find information about the configuration and calculation of RCoax systems?
Which settings do you make in LANTEK and LANTEK II from IDEAL Industries for measuring the end-to-end link of 2x2 PROFINET cables?
Which settings do you make in LANTEK and LANTEK II from IDEAL Industries for measuring PROFINET channel test profiles of 2x2 PROFINET cables?
How can you implement the the communication concept of PROFINET CBA with PROFINET IO?
Why is hardware support required for using clock-synchronized real-time communication (IRT) in PROFINET?
How is to possible to transmit real-time messages at the same time as TCP/IP communication in PROFINET?
How can real-time communication (RT) be used with standard Ethernet hardware?
What should you watch out for when reconfiguring in RUN (CiR) if the configuration contains CiR elements and a PROFINET IO system?
Which settings have to be made on the Fluke DTX-1800 cable analyzer for testing cables in a PROFINET network?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Switch on/off phase (central rack and distributed connection)
Comparison of the terms of PROFIBUS and PROFINET
Comparison of PROFINET and PROFIBUS
ET 200S (standard modules) -- Product information -- System description
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
Which hardware and software components do you need to establish communication between SIMATIC S7 stations and third-party devices using the MODBUS RTU protocol?
Which memory cards are used in the interface modules in the ET 200 with CPU functionality?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Backing up the IM 151/CPU data on Micro Memory Card
What is the meaning of the terms "sinking" (German: "P-schaltend") and "sourcing" (German: "M-schaltend") in digital modules of SIMATIC?
ET 200M (standard modules) -- Product information -- System description
Which hardware and software components do you need to establish communication between SIMATIC S7 stations and third-party devices using the MODBUS RTU protocol?
How do you replace an IM153-2 FO?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
What degree of accuracy can you obtain for plant-wide and segment-wide time stamping?
NAMUR sensors on ET200 slaves
Starting up ET200-M with analog modules
Module failure with ET200-M
What do you need the Micro Memory Card (MMC) for in the ET 200M?
Time stamping of process signal changes with IM153-2BA00
Which manuals for ET 200M are available for downloading in A&D Product Support?
ET 200eco -- Product information -- System description
Which connectors and cables can you order for the distributed IO systems ET 200eco, ET 200eco PN and ET 200pro?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
ET 200pro -- Product information -- System description
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
Which connectors and cables can you order for the distributed IO systems ET 200eco, ET 200eco PN and ET 200pro?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Industrial Ethernet network components (electrical/optical) -- Product information -- System description
How do you upgrade OpenSSL on a RUGGEDCOM APE line module (Security Advisory SSA-234763)?
How do you upgrade OpenSSL on a RUGGEDCOM APE line module (Security Advisory SSA-635659)?
How do you load the 3D, CAx and ePLAN data for the SIMATIC products?
How do you set the "Port Mirroring" function in the Industrial Ethernet switch SCALANCE X in order to monitor data transfer from a SCALANCE X port?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
Where can you find information on the topic of PROFINET?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which devices support the "Power over Ethernet" (PoE) function?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
MIB (Management Information Base) for SNMP
Dependency of bus cycle times on switch times
Industrial Ethernet S7-300/400 CPs -- Product information -- System description (protocols)
How are the communication resources assigned in the S7-300?
How do you load the 3D, CAx and ePLAN data for the SIMATIC products?
What are the differences between OPEN MODBUS / TCP Redundant V1 and OPEN MODBUS / TCP Redundant V2?
What should you watch out for when you enable the "SNMP" function in the configuration of the security module?
Which security modules support the DNS function?
What should you watch out for when enabling and using the security functions of CP343-1 Advanced and CP443-1 Advanced?
What should you watch out for when upgrading from previous modules to the successor module CP443-1 or CP443-1 Advanced?
How do you verify the authenticity of the Siemens modules CP343-1 and CP443-1?
What should you watch out for when operating a port of CP343-1, 6GK7343-1CX10-0XE0 and 6GK7343-1EX30-0XE0 with firmware V2.1 or higher, with 10 Mbit/s half duplex?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
Where do you procure the firmware extension for the CP 343-1 ERPC for database connection?
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
Which modules can you use when implementing software redundancy?
Which types of connection/protocols do the S7-300/400 CPUs and the CPs support by default?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Using C-PLUG with network components and SIMATIC CPs
What properties have the communication services and protocols that can be used in the Industrial Ethernet network?
Behavior of the communication processors during data transfer via TCP connections without RFC 1006
What should you watch out for with the ICMP Redirect (Internet control message protocol) function regarding the IP address of the router used for Industrial Ethernet CPs?
What should you pay attention to with the autonegotiation function for negotiating the LAN mode in Industrial Ethernet CPs?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
Which modules support the S7 routing function?
In the case of open TCP/IP communication via Industrial Ethernet using T blocks with IE CPs and CPUs, why are different amounts of messages sent when the maximum length of 1452 bytes of user data is transferred?
What properties, advantages and special features does the ISO protocol offer?
What properties, advantages and special features does the UDP protocol offer?
What properties, advantages and special features does the ISO-on-TCP protocol offer?
What properties, advantages and special features does the S7 protocol offer?
What properties, advantages and special features does the TCP protocol offer?
What are the requirements for disabling the PROFINET CBA interface for CP443-1EX40?
"Time Wait" with TCP connection setup
What are the different data block lengths for the various protocols of Send/Receive communication?
What is RFC1006 and what do I need this service for?
Meaning and function of the "Keep Alive" in TCP connections
S7-300 CPU 31x -- Product information -- Background and system information
What is the emergency address (emergency IP) of a CPU and when is this enabled or disabled?
All-round protection with Industrial Security - System Integrity
What are the differences between OPEN MODBUS / TCP Redundant V1 and OPEN MODBUS / TCP Redundant V2?
What is the difference between "normal routing" and data record routing?
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What should you watch out for when using the alarm numbering procedure?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
What is the maximum number of parameters that can be assigned to an FC and FB in the S7-300 CPU?
Which types of connection/protocols do the S7-300/400 CPUs and the CPs support by default?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Why is only a warm start available for S7-300?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
Which entries deal with consistent data in conjunction with distributed I/O?
What properties, advantages and special features does the S7 Basis Communication offer?
What properties, advantages and special features does the global data communication offer?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
Which modules support the S7 routing function?
How can you obtain an overview of the memory concept of SIMATIC S7-300 CPUs and C7 devices?
Retentivity behavior of S7-300 CPU 31x and complete devices C7-6xx with MMC
Status of the run-time meter after overall reset
Why does the retentivity behavior of the S7-300 CPUs and C7 devices without MMC (Micro Memory Card) influence the contents of the variables?
Local data addressing with S7-300 / S7 400
S7 300 run-time meter doesn't give any value
S7-400 CPU 41x -- Product information -- Background and system information
All-round protection with Industrial Security - System Integrity
What are the differences between OPEN MODBUS / TCP Redundant V1 and OPEN MODBUS / TCP Redundant V2?
What is the difference between "normal routing" and data record routing?
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
What should you watch out for when adding components or changing their parameters using CiR (Configuration in Run)?
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
Which types of connection/protocols do the S7-300/400 CPUs and the CPs support by default?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Behavior of the CPU after power off without back-up battery
I/O addressing with DP slaves
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
What is the difference between a restart (warm restart), cold restart and hot restart of a S7-400 CPU?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
What properties, advantages and special features does the S7 Basis Communication offer?
What properties, advantages and special features does the global data communication offer?
Which entries deal with consistent data in conjunction with distributed I/O?
What is the connection between subnet masks and IP addresses with regard to subnetting and supernetting (Classless Inter Domain Routing CIDR)?
Which modules support the S7 routing function?
CPU does not work in RUN
What does "Correction factor" mean in the "Diagnostics/Clock" tab of the CPU's Properties dialog?
What is multicomputing mode and what are the differences to operating in the segmented subrack?
Differing information on the requirement of offline/ online memory
How can I get an overview of the S7-400 memory concept?
WinAC RTX -- Product information -- System description
Which IO controllers and IO devices support the following functions: IRT, prioritized startup, MRP, PROFIenergy, Shared device, I device and clock-synchronized mode?
Which communication services supported by the CPUs with integrated PROFINET interface and by the WinAC RTX via Industrial Ethernet?
Which modules can you use when implementing software redundancy?
Which modules support the S7 routing function?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
Which SIMATIC S7 modules support the "Direct Data Exchange" function (internode communication)?
ET 200SP -- Product information -- System description
How do you load the 3D, CAx and ePLAN data for the SIMATIC products?
What is the meaning of the terms "sinking" (German: "P-schaltend") and "sourcing" (German: "M-schaltend") in digital modules of SIMATIC?
Which hardware and software components do you need to establish communication between SIMATIC S7 stations and third-party devices using the MODBUS RTU protocol?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
ET 200MP -- Product information -- System description
How do you load the 3D, CAx and ePLAN data for the SIMATIC products?
Which hardware and software components do you need to establish communication between SIMATIC S7 stations and third-party devices using the MODBUS RTU protocol?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Which PROFINET nodes support the extended PN diagnostics and what do you have to configure?
S7-1500 CPU 15xx -- Product information -- System description
What is the emergency address (emergency IP) of a CPU and when is this enabled or disabled?
Why does a program need more load memory with S7-1500 than with S7-300?
All-round protection with Industrial Security - System Integrity
How do you configure gateways on a SIMATIC S7-1500 controller?
Which S7-1500 modules support the "Routing over S7 connections" function?
Which modules support the S7 routing function?
What is the difference between "normal routing" and data record routing?
What is the meaning of the terms "sinking" (German: "P-schaltend") and "sourcing" (German: "M-schaltend") in digital modules of SIMATIC?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Why is it not possible to access a 12MB SIMATIC memory card in an internal card reader?
How do you detect an inconsistently or incorrectly formatted SIMATIC Memory Card (SMC) and how do you repair it?
SIMOTION -- Additional information -- Technical information and certificates
Dimension sheets and CAD data for SIMOTION D
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
SINAMICS/SINUMERIK/SIMOTION/SIMOTICS: UL approval
Central backplane bus of the SIMOTION C230-2.
SIMOTION D4xx: 1 GB CF card, only 512 MB usable? From where can I get the boot loader for the 1 GB CF card?
Which PROFINET nodes support automatic commissioning (device replacement without interchangeable medium) in the case of topological configuration and device replacement without topological configuration?
Part number:

Description
IO devices that support automatic commissioning (device replacement without interchangeable medium) can be easily replaced:

  • There is no need for an interchangeable medium (Micro Memory Card, for example) with saved device name.
  • The device name does not have to be assigned to the PG.

The replacement IO device no longer receives the device name from the interchangeable medium or the PG. The IO controller uses the configured topology for this and the neighbor relationships determined by the IO devices. For this all the participating devices must support the LLDP (Link Layer Discovery Protocol). The configured nominal topology must match the actual topology.

The IO controllers below support automatic commissioning (device replacement without interchangeable medium):

36752540_PROFINET_IO_Controller_list_en.pdf ( 6 KB )

The IO devices below support automatic commissioning (device replacement without interchangeable medium):

36752540_PROFINET_IO_Device_list_en.pdf ( 53 KB )

If the device name is saved in addition on the bus adapter (BA 2xRJ45 or 2xFC), you can replace it without PG and without topological configuration.
By saving on the bus adapter and on the interface module you have different scenarios when using the device name.
 
  Interface module empty Interface module with device name
Bus adapter empty No device name available Device name from interface module is used and copied to bus adapter.
Bus adapter with device name Device name from bus adapter is used and copied to interface module. Device name from bus adapter is used and copied to interface module if this has a different device name.

With the interface module below the device name is stored in addition on the bus adapter:

  • ET 200SP IM155-6 PN HF with order number 6ES7155-6AU00-0CN0

 

 Entry ID:36752540   Date:2013-07-22