|
Product information This entry contains all the SIMATIC HMI panels that have a certificate for shipbuilding from the classification societies.
Contents
- Information on the shipbuilding certificate
- Current HMI panels with shipbuilding certificate
- Discontinued HMI panels with shipbuilding certificate
Before installing the panel, note whether the panel is listed in the certificate and whether type-specific changes have to be made. Without such changes the panel does not have a shipbuilding certificate.
1. Information about the shipbuilding certificate The classification societies are responsible for classifying ships. A ship must be classified before it can sail for the merchant navy and before it can be insured along with its cargo. SIMATIC HMI Panels are certified by the following classification societies.
| Code |
Classification society |
Country |
| ABS |
American Bureau of Shipping |
USA |
| BV |
Bureau Veritas |
France |
| DNV |
Det Norske Veritas |
Norway |
| GL |
Germanische Lloyd |
Germany |
| LRS |
LIoyd's Register of Shipping |
Great Britain |
| NK |
Nippon Kaiji Kyokai |
Japan |
| PRS |
Polski Rejestr Statków |
Poland |
| RINA |
Registro Italiano Navale |
Italy |
| RMRS |
Russian Maritime Register of Shipping |
Russia |
| CCS |
China Classification Society |
China |
2. Current HMI panels with shipbuilding certificate The following panels have been certified by various shipbuilding classification societies.
Note
Note that in some panels, for example, an additional EMC filter or even lightning protection is required for the power supply for these panels to be certified. Details about shipbuilding certification are available in the relevant certificates.
The panels in the table below are currently sold by Siemens.
1) Certificates in preparation.
3. Discontinued HMI panels with shipbuilding certificate
The following panels have been certified by various shipbuilding classification societies.
Note
Note that in some panels, for example, an additional EMC filter or even lightning protection is required for the power supply for these panels to be certified. Details about shipbuilding certification are available in the relevant certificates.
The panels in the following table are discontinued and to a certain extent can no longer be procured as new parts.
Additional Keywords Classification, Shipbuilding certificate
|