show the entry list
WinCC flexible ES -- Working with projects -- Creating, editing, archiving and copying projects
Which entries are available in the internet concerning migration to STEP 7 V11 and WinCC V11 (TIA Portal)?
How can you change the column width of picture objects in WinCC flexible?
In WinCC flexible, how can you prevent pictures and picture objects being fitted automatically when you change the screen resolution (possibly widescreen)?
How do you activate access protection for a STEP 7 project and set up a user as project editor?
How do you integrate a WinCC flexible project in STEP 7?
How can you use one and the same WinCC flexible operator panel configuration for multiple controllers?
What are the solutions offered for working with different versions of WinCC flexible?
Which problems might arise if the "log.LDF" file is not available in a WinCC flexible project?
Why does WinCC flexible close again automatically after the program start?
How can you save WinCC flexible projects / libraries as projects / libraries in the format of an earlier version of WinCC flexible?
How can you delete unused tags or objects from a WinCC flexible project?
What options do you have for copying pictures from one WinCC flexible project to another?
Copying HMI projects integrated in SIMATIC STEP 7 at file level
How can you open a WinCC project integrated in STEP 7 faster?
How do you archive projects in WinCC flexible and which files are required?
How do you back transfer the projects of an operator panel and what should you watch out for?
What transfer options are available in the various operator panels?
Why does WinCC flexible close again automatically after the program start?
Part number:

Description:
The reasons for WinCC flexible closing again automatically after the program start might be the following:

  • The Trail license has expired.
  • The correct WinCC flexible license is missing.
  • An upgrade license has not been activated correctly.
  • The existing license is defective and is not recognized.

A solution to the problem points listed above and more detailed information on the topic of "Licenses" is available in Entry ID: 27005215.

 Entry ID:36660078   Date:2009-06-10 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour