show the entry list
Industrial Ethernet PC software -- Product information -- System description
How do you terminate the SINEMA Server application so that the license is no longer occupied and can be moved?
Support of SNMP variables by SIMATIC NET
Red cross in the OPC Scout Navigator
What should you watch out for in particular when implementing the Runtime Callable Wrapper (RCW) with the SIMATIC NET CD Edition 2006?
General information on the OPC server
Optimum OPC operating mode of an application
Which functions does SINEMA E provide and how do you operate SINEMA E to use them?
What is the connection between version designations of the SIMATIC NET PC software?
What should you watch out for if you change symbols in the STEP 7 project when using the OPC server of the SIMATIC NET PC software?
What are the options for connecting a PC station to Industrial Ethernet or PROFIBUS via the SIMATIC NET OPC server?
What are the special features of the changed startup behavior of the OPC data access server with SIMATIC NET CD Edition 2006?
How do I find examples, explanations and further information about SNMP and the SIMATIC NET SNMP OPC server?
PROFIBUS PC software -- Product information -- System description
Support of SNMP variables by SIMATIC NET
Red cross in the OPC Scout Navigator
What should you watch out for in particular when implementing the Runtime Callable Wrapper (RCW) with the SIMATIC NET CD Edition 2006?
What are the special features of the changed startup behavior of the OPC data access server with SIMATIC NET CD Edition 2006?
Optimum OPC operating mode of an application
What is the connection between version designations of the SIMATIC NET PC software?
What should you watch out for if you change symbols in the STEP 7 project when using the OPC server of the SIMATIC NET PC software?
Notes on using the DPC2 starting with SIMATIC NET CD 07/2001
What are the options for connecting a PC station to Industrial Ethernet or PROFIBUS via the SIMATIC NET OPC server?
What is the connection between version designations of the SIMATIC NET PC software?
Part number:

Description
There are two version designations for the SIMATIC NET PC software.

  • SIMATIC NET CD
  • Version x.y <SP> <HF>

The table below shows the connection between the version designations given above.
 
SIMATIC NET CD Version
Edition 07/2001 V6.0
Edition 07/2001 + SP1 V6.0 SP1
Edition 07/2001 + SP2 V6.0 SP2
Edition 07/2001 + SP3 V6.0 SP3
Edition 07/2001 + SP4 V6.0 SP4
Edition 07/2001 + SP5 V6.0 SP5
Edition 07/2001 + SP5 + HF2 V6.0 SP5 HF2
Edition 11/2002 V6.1
Edition 11/2002 + SP1 V6.1 SP1
Edition 11/2003 V6.2
Edition 11/2003 + SP1 V6.2 SP1
Edition 2005 V6.3
Edition 2005 + HF1 V6.3 HF1
Edition 2006 V6.4
Edition 2007 V7.0
Edition 2008 V7.1
Edition 2008 + SP2 V7.1.2
V8.0 (2010) V8.0
V8.1 (2011) V8.1
V8.2 V8.2

More information on the compatibility of SIMATIC NET PC software and Microsoft Windows operating systems is available in Entry ID: 9859007.

Additional Keywords
SOFTNET S7 Lean, S7-1613, S7-Redconnect, S7-5613, FMS-5613, DP-5613, SOFTNET-DP Slave, SOFTNET PN IO

 Entry ID:36456189   Date:2012-10-22 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour