Task: This entry shows how the function
scope of WinCC flexible and STEP 7 can be expanded by
technological blocks.
Sensors (binary and analog values) and actuators (valves,
motors) of a plant form the basis of each automation project. The
delivery scope of STEP 7 and WinCC flexible does not contain
technological blocks, to configure a basic automation, as a
standard.
At this point, this application provides a remedy. It makes
useful example blocks available for WinCC and STEP 7.
Solution:
The documentation describes how the technological blocks are
called and interconnected in STEP 7 and WinCC flexible.
This example project also shows the completed interconnection of
the technological blocks (basic automation).
- MOTOR
Visualization and operation of a motor with fixed speed and fixed
rotational direction.
- VALVE
Visualization and operation of a binary valve.
- DIGITAL
Visualization and operation of digital signals.
- ANALOGUE
Visualization and operation of analog signals.
- PIDCTRL
Visualization and operator control of a software-implemented PID
controller for regulating technical parameters with continuous
input and output values.
- MM4
Visualization and control of the frequency converter MICROMASTER
440.
- SIMODIR
Visualization and control of the motor management system SIMOCODE
Pro as direct starter.
- SIMOREV
Visualization and control of the motor management system SIMOCODE
Pro as reversing starter.
- SINAG120
Visualization and control of the frequency converter SINAMICS
G120.
Another document and project shows the possibility of dynamic
positioning during RT, and the multiple use of the technological
blocks by multiplexing addresses.
The following figure displays the most important components of
the solution.
Downloads
History
| Output |
Modifications |
| 08/2009 |
First issue ("MOTOR" block) |
| 09/2009 |
New blocks: "VALVE" and
"DIGITAL" |
| 11/2009 |
Error correction: "MotorTags" into
library element "Motor" |
| 12/2009 |
New block: "ANALOGUE" |
| 01/2010 |
New block: "PIDCtrl" |
| 03/2010 |
New block: "MM4" |
| 04/2010 |
New blocks: "SIMODIR" and
"SIMOREV" |
| 06/2010 |
New block: "SINAG120" |
| 09/2010 |
Extension: Dynamic positioning,
multiple addressed blocks |
Keywords: Faceplate
|