show the entry list
STEP 7 -- Creating HMI configurations -- Configuring alarms and messages
Why are system error messages configured with the "Report system errors" function sporadically not displayed?
What is the remedy if you cannot run diagnostics via ProAgent on the operator panel?
How do you achieve chronological messaging in STEP 7 V5.2 and higher with WinCC V6.0?
How can you optimize the runtimes of the alarm blocks and reduce the processing time in OB1?
Information about "Configuring alarms and messages"
What is the difference between CPU-wide messages and project-wide messages and how do you configure symbol-related messages?
WinCC flexible Options -- Product information -- WinCC flexible / ProAgent
What support does Siemens AG offer to make the use of WinCC flexible comply with FDA regulations?
What is the remedy if you cannot run diagnostics via ProAgent on the operator panel?
What should you watch out with regard to licenses for WinCC flexible and panels?
WinCC flexible ES -- Operation and maintenance -- Diagnosing errors
How do you use the "SIMATIC Diagnostics Tool" (SDT2012) to collect diagnostics and system data?
How do you use the "SIMATIC Diagnostics Tool" (SDT2011) to gather together the diagnostics and system information of multiple computers on one computer?
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?
What is the remedy if you cannot run diagnostics via ProAgent on the operator panel?
Touch Panel / Operator Panel -- Creating HMI configurations -- Configuring alarms and messages
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
What is the remedy if you cannot run diagnostics via ProAgent on the operator panel?
Two-line messages with S7-PDIAG and OP27/TP27
How do you display ALARM_S or ALARM_D messages with process values (so-called associated values) on a WinCC flexible operator panel?
Multi Panel -- Creating HMI configurations -- Configuring alarms and messages
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
What is the remedy if you cannot run diagnostics via ProAgent on the operator panel?
How do you display ALARM_S or ALARM_D messages with process values (so-called associated values) on a WinCC flexible operator panel?
What is the remedy if you cannot run diagnostics via ProAgent on the operator panel?
Part number:

Description:
Proceed as follows if, after dearchiving a STEP 7 project and then transferring the data, you cannot run diagnostics via ProAgent on the operator panel and you get an error message indicating that there is an error in the diagnostics block.

Remedy:
Check whether the diagnostics data of ProAgent in WinCC flexible are correctly activated (under "Project > Diagnostics > ProAgent"). If not and there is no diagnostics data, you have to reinsert the station for communication in the "Connections" dialog. The procedure for this is described in the table below:
 
No. Procedure:
1 In WinCC flexible you open the dialog "Project > Communication > Connections" and open the drop-down menu under "Station" as shown in Fig. 01. Select the item "No station".


Fig. 01

2 In the "Connections" dialog, you reopen the drop-down menu under "Station" and reinsert your station as shown in Fig. 02.


Fig. 02

3 The diagnostics data is once again available in the dialog "Project > Diagnostics > ProAgent". Activate the associated name of the connection as shown in Fig. 03 (example: "Verbindung_1" (Connection_1")).


Fig. 03

4 In WinCC flexible, you compile the configuration with the menu command "Project > Generator > Generate".
5 Then open the "Select devices for transfer" dialog via "Project > Transfer > Transfer settings..." and check your settings:
  • Mode (e.g. Ethernet)
  • Computer name or IP address
6 Click on the "Transfer" button to download the data for WinCC flexible and ProAgent to the operator panel. Now it is possible to run diagnostics again.

 Entry ID:36078949   Date:2009-08-06 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour