show the entry list
WinAC RTX -- Product information -- Information on previous versions
Automatic minimizing of window for WinLC when starting up
What connections are there between the version designations in WinAC RTX?
Access via MPI card to external S7 CPU
WinAC: configuring the CP5412-A2 with the DP database (CP_L2_1.ldb)
Error message in the compiler of Visual Basic when using S7 Number Control
Diagnostics buffer of the soft container displays only "###" instead of message texts.
WinLC V3.0 sporadically goes into the "Defective" state
Using Operator Panel of the WinLC RTX in the soft container or of a VB application
WinAC with STEP 7 - Mini
Access to a WinLC on a remote PC via PROFIBUS
Request for overall reset after logging on in Windows NT under a different user name
How many connections can you set up to a WinAC Basis V3.x and WinAC RTX V3.x?
Communications between WinAC RTX (with CP 5613) and OP
WinAC RTX F -- Product information -- Information on previous versions
Automatic minimizing of window for WinLC when starting up
What connections are there between the version designations in WinAC RTX?
WinLC V3.0 sporadically goes into the "Defective" state
How many connections can you set up to a WinAC Basis V3.x and WinAC RTX V3.x?
What connections are there between the version designations in WinAC RTX?
Part number:

Description:
As of 2005, the versions of SIMATIC WinAC RTX are designated by year numbers. These product designations are not listed in the Hardware Configuration of STEP 7. Therefore, there are differences between the

  • Product designation
  • Version designation in the information dialog of the WinLC RTX Controller Panel
  • Version designation in the STEP 7 Hardware Configuration

Overview of version designations:
The table below gives an overview of the versions as from WinAC RTX 2005.
 

Product designation

Designation in the information dialog Designation in the Hardware Configuration
WinAC RTX 2005 V4.2.0 V4.2
WinAC RTX 2005 + SP1 V4.2.1 V4.2
WinAC RTX 2005 + SP2 V4.3.0 V4.3
WinAC RTX 2008 V4.4.0 V4.4
WinAC RTX 2008 + SP1 V4.4.1 V4.4
WinAC RTX 2009 V4.5.0 V4.5
WinAC RTX F 2009 V4.5.0 V4.5
WinAC RTX 2010 V4.6.0 V4.6
WinAC RTX F 2010 V4.6.0 V4.6

Instructions:
Proceed as follows to determine which version of WinAC RTX is installed on your computer.

  1. Open the WinLC RTX Controller Panel via:
    Start > SIMATIC > PC Based Control > WinLC RTX
     
  2. Via the menu command Help > About, you open the dialog containing information about the version of the software.


    Fig. 01

You must perform the following two tasks to select the correct version of WinLC RTX in the Hardware Configuration.

  1. Compare the version in this About dialog with the table above.
     
  2. Select the relevant entry from the table in the Hardware Configuration.


    Fig. 02

 Entry ID:36059839   Date:2011-07-20 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour