show the entry list
WinCC flexible RT -- Product information -- General information
What support does Siemens AG offer to make products comply with FDA regulations?
Why does the "Lock program switching" function no longer work after upgrading from SIMATIC WinCC flexible Runtime 2008 SP2 to SP3?
What new features do Intel® Atom™ processors have and what advantages do SIMATIC IPCs with Intel® Atom™ processors offer when used with SIMATIC software?
Which licenses do you need to upgrade from WinCC flexible 2008 or WinCC V7 to WinCC V11 and in WinCC V11?
What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook?
How resistant to chemicals are the SIMATIC HMI operator panels and Industrial PCs?
What options are there for creating a screenshot in WinCC flexible ES, WinCC flexible Runtime or on panels?
What support does Siemens AG offer to make use of WinCC flexible, WinCC flexible Runtime and panels that can be configured with WinCC flexible comply with FDA regulations?
What should you watch out with regard to licenses for WinCC flexible and panels?
How do you have csv archive files exported from WinCC flexible RT or a panel displayed graphically on the PC?
Which ports are used by WinCC flexible?
WinCC flexible Options -- Product information -- WinCC flexible /Sm@rtService (Teleservicing)
Why do you get an error message when opening the Sm@rtClient with the internet browser?
What options are there for creating a screenshot in WinCC flexible ES, WinCC flexible Runtime or on panels?
How do you have csv archive files exported from WinCC flexible RT or a panel displayed graphically on the PC?
How can you use a PC to simulate or realize sending e-mails in the case of an HMI station message?
What should you watch out with regard to licenses for WinCC flexible and panels?
What are the options for remote maintenance of a WinCC flexible Runtime system (Panel/PC) via the Internet (WAN)?
Connection to the SIMATIC WinCC flexible Sm@rtServer gets lost (with active screensaver or "Shut Down")
Why are not all the tabs visible under "Internet Settings" of the SIMATIC operator panels (only Windows CE devices)?
Why do you get the message "Under Construction" in WinCC flexible when attempting to connect to the MiniWeb with the HTML viewer?
Why, when you call the Sm@rtClient, is only an empty page displayed in the Internet Explorer?
How do you send e-mails from a Windows CE panel or PC with SIMATIC WinCC flexible?
How do you send short messages (SMS) from an SIMATIC WinCC flexible HMI station to a mobile phone?
WinCC flexible ES -- Creating HMI configurations -- Using archives
How do you use a script to determine whether a storage drive with removable media (USB stick, SD/MMC card) is ready for writing on an HMI device?
How can you safely copy or move archives in WinCC flexible?
How can you output batch data or archived data via an HMI operator panel?
How do you do long-term archiving with WinCC flexible?
How can you output tags from an SQL database via a trend archive?
What special points are there in the WinCC flexible function "Archive log file" in the "Move" mode?
How do you have csv archive files exported from WinCC flexible RT or a panel displayed graphically on the PC?
How can you have a trend archive displayed continuously updated after calling Trend View?
What do you need to watch out for when naming archives and when archiving tags in a csv file on Windows-based systems?
How can you store tags/data records event-triggered with date and time in a CSV file?
How are tags archived in WinCC flexible STRING?
Which external storage locations are available on the various operator panels (TIA Portal/WinCC flexible/ProTool) for archiving data?
How are tags and alarms logged in WinCC flexible?
How do you log tags in an SQL database and read them out again with WinCC flexible?
How can you have data from a tag log displayed in table form for panels or the WinCC flexible PC Runtime?
How can you read texts from and write texts to a CF card with a Windows CE Panel?
Micro Panels -- Operation and maintenance -- Saving data
How do you have csv archive files exported from WinCC flexible RT or a panel displayed graphically on the PC?
How do you backup/restore with a Windows-based panel?
How can you make a project backup from an operator panel?
Mobile Panels -- Operation and maintenance -- Saving data
How do you backup/restore with a Windows-based panel?
How do you have csv archive files exported from WinCC flexible RT or a panel displayed graphically on the PC?
How can you make a project backup from an operator panel?
Exporting a password list without path specification
Touch Panel / Operator Panel -- Operation and maintenance -- Saving data
How do you backup/restore with a Windows-based panel?
How do you have csv archive files exported from WinCC flexible RT or a panel displayed graphically on the PC?
How can you make a project backup from an operator panel?
Exporting a password list without path specification
Multi Panel -- Operation and maintenance -- Saving data
How do you backup/restore with a Windows-based panel?
How do you have csv archive files exported from WinCC flexible RT or a panel displayed graphically on the PC?
How can you make a project backup from an operator panel?
Exporting a password list without path specification
WinCC flexible Options -- Product information -- WinCC flexible /Archives
What support does Siemens AG offer to make products comply with FDA regulations?
What support does Siemens AG offer to make use of WinCC flexible, WinCC flexible Runtime and panels that can be configured with WinCC flexible comply with FDA regulations?
How do you have csv archive files exported from WinCC flexible RT or a panel displayed graphically on the PC?
What should you watch out with regard to licenses for WinCC flexible and panels?
How do you have csv archive files exported from WinCC flexible RT or a panel displayed graphically on the PC?
Part number:

Introduction
In Runtime mode of WinCC flexible the tag values can be stored in archives and evaluated at later. These tag archives are difficult to read outside the panel and cannot be evaluated graphically without WinCC.

Solution
Entry ID 60520367 provides an Excel application for analyzing archives generated with WinCC (TIA Portal). This tool is compatible with archives generated with WinCC flexible configurations.

 Entry ID:35929465   Date:2014-05-21