|
QUESTION:
Which Safety Integrity Level SIL acc. to IEC 61511 is attainable with subsystems or subsystem elements consisting of SIRIUS electromechanical components with low demand mode according to IEC 61508 ?
ANSWER:
IEC 61511 – Application Explanations: Possible attainable SIL of subsystems or subsystem elements consisting of SIRIUS electromechanical components with low demand mode (defined in accordance with IEC 61508)
The explanations in attached document are to address these issues.
Anymore questions?
Please consult Siemens Low Voltage Switchgear - Technical Assistance via mail adress or phone number, as shown in the header of the attached document.
IEC61511_Info_1_en.pdf ( 43 KB )
|