Product description: A Thin Client is an industry-compatible panel that is permanently connected to a server via Ethernet and on which no local applications run (except for the integrated browser). All Thin Clients receive the operator display from the server sent via the network and show this operator display without the applications being installed on the Thin Clients themselves. Entries on the Thin Client are transferred to the server and processed accordingly. Operation on the Thin Client is the same as if you were operating on the server itself.
The Thin Client supports the following connections:
- Sm@rtAccess
- RDP
- HTTP (via web browser)
Download:
The following PDF document includes a compilation of possible Thin Client applications.
Attachment 1: Thin_Client_Application_possibilities_e.pdf ( 1011 KB )
Keywords:
RDP = Remote Desktop Protocol, Sm@rtAccess server, Sm@rtAccess clients
|