show the entry list
S7-300 CPU 31x -- Product information -- Technical data
How can you control the ALM (Active Line Module) of a CU320 (with DriveCLIQ) with the SIMATIC program?
Where can you find an update to use the SINAMICS with newer firmware in S7 Technology V4.1?
Which modules can you use when implementing software redundancy?
Which organization blocks do you have to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails?
How do you find out further technical information about your module?
Why can't I see the values which are transmitted to an unlinked destination DB with SFC84, even though SFC84 is not indicating an error (RET_VAL = W#16#000?
How does the CPU 31x/31xC/C7 react when an MMC fault occurs during the save procedure?
What is the effect of the STEP 7 function "Copy RAM to ROM"?
Why does the SFC 54 "RD_DPARM" not work with the new S7-300 CPU with MMC?
How do you copy the user program from the load memory into the main memory without PG with a S7-300 CPU with MC slot?
How can you backup your program from the load memory?
Which communication services supported by the CPUs with integrated PROFINET interface and by the WinAC RTX via Industrial Ethernet?
Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas
At which ambient temperature and at which air pressure can you operate a SIMATIC S7-300?
What can you do when the power requirement of the modules in the subrack exceeds the power supply provided by the CPU on the backplane bus?
Where do you find certificates and approvals for SIMATIC S7 in the Internet?
Where can you find images, graphics, symbols and screenshots for SIMATIC industrial automation systems?
Which SIMATIC S7 components and which drives support clock-synchronicity functionality?
S7-400 CPU 41x -- Product information -- Technical data
What are the functional restrictions of old releases and firmware versions for the S7-400 CPUs operating in conjunction with the CP443-5 Extended V6.1?
Which modules can you use when implementing software redundancy?
Which organization blocks do you have to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails?
How do you find out further technical information about your module?
Which communication services supported by the CPUs with integrated PROFINET interface and by the WinAC RTX via Industrial Ethernet?
Implementation of SIMATIC modules of the product families S7-300, S7-400, ET 200M, ET 200S ET, 200iSP and TDC in environments with high concentrations of corrosive gas
Where can you find images, graphics, symbols and screenshots for SIMATIC industrial automation systems?
Where do you find certificates and approvals for SIMATIC S7 in the Internet?
Which SIMATIC S7 components and which drives support clock-synchronicity functionality?
Retentivity behavior of S7-400 CPUs and the CPU 318-2 CPUs
S7-400: Operating Mode Switch at the new CPU 41x (as of FW Version 4.0)
How do you find out further technical information about your module?
Part number:

Description:
In the following you will be shown how to access detailed technical data about the module you use. This is done using an S7-300 CPU315 as an example.

First of all, enter the name of the module you use (without its version designation, e.g.: CPU314, SM322, CP343, ET200S, ...) in the search line:


Fig. 01

While you are making your input, a product link window, which is shown in Fig. 2, appears to the left of the search line. The modules which match the keyword appear here. Now look for the module you use on the basis of the order number.


Fig. 02

Notes:

  • If the list in Fig. 2 does not include the module which you use, this indicates that this module has been phased out for a number of years. In this case, there will be no further technical information available.
  • Alternatively, you can also enter the start of an order number (e.g. 6es7315) instead of a module name.

Now left-click the module you use in the product link window. The corresponding product information then appears. It is shown in Fig. 3.


Fig. 03

You can find the following information, among others, in the Entries tab:

  • Downloads
  • FAQs
  • Certificates
  • Manuals and operating instructions
  • Applications

You can find further information about the module which you use in the Technical Data tab.

 Entry ID:35113490   Date:2009-04-06 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour