Configuration Notes: The EU conformity declarations
are intended solely for the relevant authorities (in Germany it is
the "Regulatory Authority for Telecommunications and Post - Reg
TP"). By affixing the CE mark, we confirm that the product
properties conform to the relevant EU guidelines (e.g. the EMC
directive).
The EC conformity declarations for SIMATIC HMI products are filed
in the following department:
Siemens Aktiengesellschaft
Automation Environment
Dept. A&D AS HMI BD
P.O. Box 4848
D-90327 Nürnberg
Keywords: OP3, OP7, OP17, OP27, TP27, OP37, TP37,
OP170, TP170, Mobile panel 170, OP270, TP270, MP270, MP370, Touch,
Multi panel, Operator panel, Windows-based panels, Text panels,
Graphic devices, Line-oriented panels, WINCE, Windows CE, PC,
Certificates, Directives, EU test identifier
|