show the entry list
Industrial Ethernet S7-300/400 CPs -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
What should you watch out for when a MAC address is entered for the PROFINET interface or GBIT interface in the configuration of the Industrial Ethernet CP343-1/CP443-1?
How do you configure a shared device when you are using a CPx43-1 Advanced as PROFINET IO controller and the GBIT interface of the module is networked?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Which Industrial Ethernet CPs support the DHCP Option 12 (Host Name) and how do you configure the DHCP Option 12?
What should you watch out for when parameterizing the watchdog time when a ring redundancy is established with the Media Redundancy Protocol?
How do you use an Industrial Ethernet CP or SCALANCE S as a gateway?
How do you disable the "Link Layer Discovery Protocol" function at the ports of an IE CP of S7-300 or S7-400?
Where can you find sample S7 programs and documentation for communication via gateways and network components, and for security in networks on the SIMATIC NET Quick Start Collection?
What should you watch out for when operating a CP443-1EX20 V2.0 on a CPU V5.1?
Changing the configuration data of users for CP 343-1 IT and CP 443-1 IT
Loading the configuration via LAN into the IE-CP in "STOP" mode
Special points when setting the LAN medium for Industrial Ethernet CPs
Starting up automation systems with Industrial Ethernet without previous node initiation via MPI
Rejected diagnostics connection via TCP/IP protocol after changing the MAC address
Establishing an online connection to an S7-300/S7-400 CPU through several Ethernet interfaces
What should you pay attention to when formatting the file system in the S7-300 and S7-400 Industrial Ethernet CPs?
What should you watch out for when replacing the CP443-1 (6GK7443-1EX11-0XE0) with a CP443-1 (6GK7443-1EX20-0XE0 V1.0) in STEP 7 V5.4 SP3?
What is the meaning of the configuration option "Activate Web server" with CP443-1 EX20?
Why with CP443-1 Advanced is a different firmware version than the module displayed in the C-PLUG info text in the NCM S7 Diagnostics?
Which options are available for assigning the PROFINET IO controller a new IP address?
How can you configure an S7 CP during runtime?
How do you disable the S7 routing functions?
Which manufacturer ID, in other words OUI (Organizationally Unique Identifier), does SIEMENS AG use for the MAC addresses of network-compatible devices?
How can you protect the S7-300/400 against unauthorized access from the LAN (local area network)?
What should you watch out for when using the function block FB55 "IP_CONFIG" to configure an Industrial Ethernet CP?
Why are some of the newer versions of the names of SIMATIC NET modules not used in the hardware catalog?
Why can't my SIMATIC S7-300 Ethernet CP run as many S7 communication connections as specified?
How does connection multiplexing work and how do you configure it for SIMATIC S7-300 Ethernet CPs?
What should you watch out for when operating a CP443-1EX20 V2.0 on a CPU V5.1?
Part number:

Description:
In a SIMATIC S7-400 station, the CP443-1EX20 with firmware V1.0 is operated on a CPU V5.1, for example CPU 414-3PN/DP. The CP443-1EX20 version V1.0 and the CPU version V5.1 are configured in the STEP 7 Hardware Configuration. The CP443-1 EX20 is operated as PROFINET IO controller.

After configuration of the S7-400 Station and the PROFINET IO system, the configuration is loaded into the CPU of the S7-400 station. It is now possible to exchange data between the CP443-1EX20 as PROFINET IO controller and the PROFINET IO devices connected. You can stop and start the components. The whole configuration can be loaded multiple times.

If the CP443-1EX20 V1.0 is defective, you can use the CP443-1EX20 V2.0 as spare part without changing the configuration in STEP 7.

Special feature
Startup problems might occur in the constellation described. This occurs sporadically when the configuration is loaded.
The configuration is reloaded if the CP is already in RUN mode. In this case, the load process might be aborted. The CP can no longer be reached via the LAN.

In the CPU's diagnostics buffer you are informed of the event by the following entries. The "no connection" fault type and the specified slot indicate the CP.

Excerpt from the CPU's diagnostics buffer
Event 14 of 133: Event ID 16#6547
Parameter error when parameterizing modules (not via P bus, but abort of download)
not user-relevant: SDB number : 3000
Type of fault: no connection or disconnection
Module affected in subrack 0 and slot 10
Mode: STOP (internal)
internal error, incoming event

Remedy
There are the following possible remedies for the case described.

  • Upgrade the CPU's firmware to version V5.2 or higher.
  • Switch off the power supply. Switch on the power supply again and you can reload the configuration. After successful completion of the download, the S7-400 station starts to operate again. Note that the startup problem might reoccur with future download processes.

Note:
Entry ID 24890935 contains among other things information on the compatibility between S7-400 CPU and CP443-1EX20.

 Entry ID:34677120   Date:2009-03-20 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour