Description: When using Save as... with the option Reorganization (slow) or you copy/paste a SIMATIC station in the SIMATIC Manager, you might get the error message "Invalid file position".

Fig. 01
When should you expect this behavior? This behavior can occur in a project that you have created or processed with PCS 7 as from V7.0 SP1 and F Systems V6.0. It might happen that the "Invalid file position" is output with the following actions:
- If the project is stored in the SIMATIC Manager using Save As with Reorganization (slow).
- If the complete SIMATIC station is copied and pasted in the SIMATIC Manager.
How can you avoid this behavior? There are three ways of avoiding this behavior.
- Implement F Systems V6.1.
OR
- Run the actions concerned on an Engineering Station on which F Systems V6.0 is not installed (the F Configuration Pack must be installed).
OR
- When implementing PCS 7 V7.0 SPx (and using F Systems V6.0), run the attached file "S7F-Wrp.EXE" once on the Engineering Station concerned. Now, the actions concerned can be completed successfully after restarting the SIMATIC Manager.
S7F-Wrp.zip ( 39 KB )
Keywords:
Safety integrated, Process safety
|