show the entry list
Industrial Ethernet S7-300/400 CPs -- Configuring and programming communication -- Using communication blocks
How do you use the predefined data type UDT1 "FILE_DB_HEADER" for FTP communication in the S7-300 and S7-400?
How do you enable the ad-hoc mode when you call the TRCV instruction?
How do you use the blocks for MODBUS/TCP communication over an Industrial Ethernet CP of S7-300 and S7-400 in STEP 7 Professional (TIA Portal)?
How do you copy the CFC chart "Modbus" from the sample project for OPEN MODBUS / TCP into your user project?
What is the difference between the initialization and runtime parameters on the blocks for Modbus TCP?
Why is the status value A090 (hex) output for Modbus TCP although you have entered the correct license?
What are the differences between the licensed version and the downloadable demo version of the blocks for Modbus TCP?
Why is the value A083 (hex) output permanently at the STATUS output parameter of the block for Modbus TCP when the ENQ_ENR=true input parameter has been set?
How is data with variable message length transferred via the TCP protocol and received by an S7-300 station via the Industrial Ethernet CP?
How do you program the function blocks FB14 "GET" and FB15 "PUT" in the S7 program of the S7-300 in order to transfer more than 160 bytes of data?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules via Industrial Ethernet using the UDP protocol?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules via Industrial Ethernet using the TCP protocol?
Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules via Industrial Ethernet using the ISO transport protocol?
How do you program the FC10 "AG_CNTRL"?
Which commands (CMD) of the FC10 "AG_CNTRL" are supported by the IE CPs?
How many communication jobs may be used simultaneously in an S7-300 CPU for S7 communication via a CP343-1?
Which ports are released for Modbus/TCP communication and how many Modbus clients can communicate with a SIMATIC S7 CPU as Modbus server?
Notes on using an instance for multiple connection IDs
Internal call of FC5 (AG_SEND) with FTP client blocks (FC 40-44) for the CP343-1 IT (6GK7 343-1GX11-0XE0)
How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the ISO-on-TCP protocol for data exchange via the integrated PROFINET interface of an S7-300/S7-400 CPU or via the CP443-1 Advanced?
How do you program communication blocks FC11 and FC12 for the PROFINET IO device?
Block calls for communications processors in multiple runtime layers
Changing the input parameter of the user blocks "AG_SEND" and "AG_RECV" during the runtime of a job
What should you watch out for if you transfer variables with the data type "REAL" when calling the communication blocks FC5/50 "AG_SEND/AG_LSEND" and FC6/60 "AG_RCV/AG_LRCV"?
What should you pay attention to when using the communication blocks FC53 "AG_SSEND" and FC63 "AG_SRECV"?
What points do you need to remember when calling communication blocks FC5/50 and FC6/60 in the STEP 7 user program of the CPU?
How do you program communication blocks FC11 and FC12 for the PROFINET IO controller?
How do you establish OPEN MODBUS / TCP communication from a SIMATIC S7 and where can you find further information?
How do you program the communication blocks FC50 and FC60?
Error STATUS "0x7000" on function block FC6 / FC60 (AG_SEND) with Send/Receive communication on the S7-400 controller
How do you program the communication blocks FC5 and FC6?
Sample program: S7 communication with the blocks SFB14 ("GET") and SFB15 ("PUT") with S7-400
Sample Program: S7 Communication with blocks FB14 ("GET") und FB15 ("PUT") of the CPU 317-2PN/DP
How do you program communication blocks FB8 "USEND" and FB9 "URCV" for data exchange on the S7-300?
"STATUS = 27" (0x001B) with the loadable S7 communication on the S7-300
How do you program communication blocks FB14 "GET" and FB15 "PUT" for data exchange in the S7 program of an S7-300 CPU?
How do you program communication blocks FB12 "BSEND" and FB13 "BRCV" for data exchange in the S7 program of an S7-300 CPU?
Repeating the "BSEND" job (SFB12) when the "BRCV" block (SFB13) is in the "disabled" state ("EN_R = 0")
S7-300 CPU 31x -- Configuring and programming communication -- Using communication blocks
In STEP 7 V5.5, how do you read out the IP address of the S7-300 CPU in the user program?
What is the volume of data that you can transfer with function blocks FB34 "GET_E" and FB35 "PUT_E"?
How do you cyclically read out the 8 channels of the FM 350-2 counter module as quickly as possible?
How do you read out the IP address of the S7-300 CPU in the user program at runtime?
How do you enable the ad-hoc mode when you call the TRCV instruction?
How do you use the blocks for MODBUS/TCP communication over the integrated PROFINET interface of the CPU in STEP 7 Professional (TIA Portal)?
Which security modules can be reached with SOFTNET Security Client V4 over a secure IPsec tunnel connection?
What is the difference between the initialization and runtime parameters on the blocks for Modbus TCP?
Why is the status value A090 (hex) output for Modbus TCP although you have entered the correct license?
What are the differences between the licensed version and the downloadable demo version of the blocks for Modbus TCP?
Why is the value A083 (hex) output permanently at the STATUS output parameter of the block for Modbus TCP when the ENQ_ENR=true input parameter has been set?
Which blocks for Modbus TCP can you rename or re-wire when the block numbers of the Modbus blocks are already being used in the user program?
How do you implement chronological messaging with S7-300 CPUs and WinCC?
How do you program communication blocks FB14 "GET" and FB15 "PUT" for data exchange in the S7 program of an S7-300 CPU?
How can you read out diagnostics data from a SIRIUS 3RK3 modular safety system using a S7-300/400 CPU?
Which ports are released for Modbus/TCP communication and how many Modbus clients can communicate with a SIMATIC S7 CPU as Modbus server?
How do you configure a specified and an unspecified S7 connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs?
What restrictions are there for active jobs when communicating with SFC 58 / SFC 59 and SFB 52 / SFB 53 via PROFIBUS DP and PROFINET IO?
How do you program communication blocks FB12 "BSEND" and FB13 "BRCV" for data exchange in the S7 program of an S7-300 CPU?
How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the ISO-on-TCP protocol for data exchange via the integrated PROFINET interface of an S7-300/S7-400 CPU or via the CP443-1 Advanced?
How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the TCP protocol for data exchange by means of the integrated PROFINET interface of an S7-300/S7-400 CPU?
How do you establish OPEN MODBUS / TCP communication from a SIMATIC S7 and where can you find further information?
How do you program the communication blocks FB67 "TUSEND", FB68 "TURCV", FB65 "TCON" and FB66 "TDISCON" in order to use the UDP protocol for data exchange via the integrated PROFINET interface of an S7-300/S7-400 CPU?
How does data communication work between S7-300/S7- 400 and S7-200 via MPI using S7 basic communication?
How great is data consistency in the PUT and GET S7 communication functions for the individual S7-300 CPUs and C7 complete devices?
How can you access via PROFIBUS DP another CPU, which is connected to the PROFIBUS DP as a slave, from a DP master using basic communication with SFC72 "I_GET" and SFC73 "I_PUT"?
How can you access consistent data without SFC14/15 as part of the process image?
S7-400 CPU 41x -- Configuring and programming communication -- Using communication blocks
When using the FB81 S_MODB on an S7-400 with more than 8 Kbytes of marker, how do you access the marker area above MB 255?
How do you enable the ad-hoc mode when you call the TRCV instruction?
How do you use the blocks for MODBUS/TCP communication over the integrated PROFINET interface of the CPU in STEP 7 Professional (TIA Portal)?
How do you establish a redundant MODBUS/TCP communication over the integrated PROFINET interface of a CPU 41x-H in STEP 7 V5.5?
What is the difference between the initialization and runtime parameters on the blocks for Modbus TCP?
Why is the status value A090 (hex) output for Modbus TCP although you have entered the correct license?
What are the differences between the licensed version and the downloadable demo version of the blocks for Modbus TCP?
Why is the value A083 (hex) output permanently at the STATUS output parameter of the block for Modbus TCP when the ENQ_ENR=true input parameter has been set?
Which blocks for Modbus TCP can you rename or re-wire when the block numbers of the Modbus blocks are already being used in the user program?
How can you read out diagnostics data from a SIRIUS 3RK3 modular safety system using a S7-300/400 CPU?
Which communication options are there in SIMATIC S7?
How does data communication work between S7-300/S7- 400 and S7-200 via MPI using S7 basic communication?
Consistent data in S7-400, summary of mechanisms
Which ports are released for Modbus/TCP communication and how many Modbus clients can communicate with a SIMATIC S7 CPU as Modbus server?
How do you implement chronological messaging with S7-400 CPUs and WinCC?
How do you configure a specified and an unspecified S7 connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs?
How do you establish OPEN MODBUS / TCP communication from a SIMATIC S7 and where can you find further information?
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?
What restrictions are there for active jobs when communicating with SFC 58 / SFC 59 and SFB 52 / SFB 53 via PROFIBUS DP and PROFINET IO?
How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the ISO-on-TCP protocol for data exchange via the integrated PROFINET interface of an S7-300/S7-400 CPU or via the CP443-1 Advanced?
How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the TCP protocol for data exchange by means of the integrated PROFINET interface of an S7-300/S7-400 CPU?
How do you program the communication blocks FB67 "TUSEND", FB68 "TURCV", FB65 "TCON" and FB66 "TDISCON" in order to use the UDP protocol for data exchange via the integrated PROFINET interface of an S7-300/S7-400 CPU?
How can you access consistent data without SFC14/15 as part of the process image?
How great is data consistency in the PUT and GET S7 communication functions for the individual S7-400 CPUs?
ET 200S (standard modules) -- Configuring and programming communication -- Using communication blocks
When using the FB81 S_MODB on an S7-400 with more than 8 Kbytes of marker, how do you access the marker area above MB 255?
How do you set the input parameter TIME_RTS_OFF of the S_V24 instruction in the case of low data transfer rates?
How do you use the ET200S 1SI module in conjunction with a CPU S7-15xx?
How in WinAC MP 2008 do you program data transfer with the ET200S 1SI module for the 4-byte or 8-byte communication type?
Which CPU can you operate as a PROFINET I device?
What restrictions are there for active jobs when communicating with SFC 58 / SFC 59 and SFB 52 / SFB 53 via PROFIBUS DP and PROFINET IO?
Which ports are released for Modbus/TCP communication and how many Modbus clients can communicate with a SIMATIC S7 CPU as Modbus server?
How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the TCP protocol for data exchange by means of the integrated PROFINET interface of an S7-300/S7-400 CPU?
How do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the ISO-on-TCP protocol for data exchange via the integrated PROFINET interface of an S7-300/S7-400 CPU or via the CP443-1 Advanced?
How do you program the communication blocks FB67 "TUSEND", FB68 "TURCV", FB65 "TCON" and FB66 "TDISCON" in order to use the UDP protocol for data exchange via the integrated PROFINET interface of an S7-300/S7-400 CPU?
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?
"Report System Errors" function can be used with ET 200S CPU from firmware version V2.1
Using the SFB75 (send alarm to the DP master) on an ET 200S CPU
Which ports are released for Modbus/TCP communication and how many Modbus clients can communicate with a SIMATIC S7 CPU as Modbus server?
Part number:

Ports released for Modbus/TCP communication
The following ports are used by the Modbus/TCP protocol.

  • By default, the protocol uses Port 502 as local port in the Modbus server.
  • You can set the local port as you wish in the Modbus client. Usually, port numbers starting at 2000 are used.

If the communication partners offer the option of setting the port numbers for the server, then it is also possible to communicate using the Modbus/TCP protocol through a port other than Port 502.

If you use the SIMATIC as Modbus server, then there are restrictions for a number of CPUs regarding the released port numbers.
The following port numbers are released for the local port:
 
CPU Order number Firmware version Released ports Multiport
IM 151-8(F) PN/DP CPU 6ES7151-8AB00-0AB0
6ES7151-8FB00-0AB0
up to V2.6 2000 to 5000 No
IM 151-8(F) PN/DP CPU 6ES7151-8AB00-0AB0
6ES7151-8FB00-0AB0
from V2.7 all No
IM 151-8(F) PN/DP CPU 6ES7151-8AB01-0AB0
6ES7151-8FB01-0AB0
from V3.2 all Yes
IM 154-8 PN/DP CPU 6ES7154-8AB00-0AB0 up to V2.5 2000 to 5000 No
6ES7154-8AB01-0AB0 from V3.2 all Yes
IM 154-8F PN/DP CPU 6ES7154-8FB01-0AB0 from V3.2 all Yes
IM 154-8FX PN/DP CPU 6ES7154-8FX00-0AB0 from V3.2 all Yes
CPU 314C-2 PN/DP 6ES7314-6EH04-0AB0 from V3.3 all Yes
CPU 315(F)-2PN/DP 6ES7315-2EG10-0AB0
6ES7315-2EH13-0AB0
6ES7315-2FH10-0AB0
6ES7315-2FH13-0AB0
up to V2.3.4 2000 to 5000 No
CPU 315(F)-2PN/DP 6ES7315-2EH14-0AB0
6ES7315-2FJ14-0AB0
from V3.1 all Yes
CPU 315T-3 PN/DP 6ES7315-7TJ10-0AB0 from V3.2 all Yes
CPU 317(F)-2PN/DP 6ES7317-2EK13-0AB0
6ES7317-2FK13-0AB0
up to V2.3 2000 to 5000 No
CPU 317(F)-2PN/DP 6ES7317-2EK14-0AB0
6ES7317-2FK14-0AB0
from V3.1 all Yes
CPU 317T-3 PN/DP 6ES7317-7TK10-0AB0 from V3.2 all Yes
CPU 317TF-3 PN/DP 6ES7317-7UL10-0AB0 from V3.2 all Yes
CPU 319(F)-3PN/DP 6ES7318-2EL00-0AB0
6ES7318-2FL00-0AB0
up to V2.6 2000 to 5000 No
CPU 319(F)-3PN/DP 6ES7318-2EL00-0AB0
6ES7318-2FL00-0AB0
from V2.7 all No
CPU 319(F)-3PN/DP 6ES7318-2EL01-0AB0
6ES7318-2FL01-0AB0
from V3.2 all Yes
CPU 412-2 PN 6ES7412-2EK06-0AB0 from V6.0 all Yes
CPU 414-3PN/DP 6ES7414-3EM05-0AB0 from V5.0 all No
CPU 414(F)-3PN/DP 6ES7414-3EM06-0AB0
6ES7414-3FM06-0AB0
from V6.0 all Yes
CPU 416(F)-3PN/DP 6ES7416-3ER05-0AB0
6ES7416-3FR05-0AB0
from V5.0 all No
CPU 416(F)-3PN/DP 6ES7416-3ES06-0AB0
6ES7416-3FS06-0AB0
from V6.0 all Yes
CPU 412-5H PN/DP 6ES7412-5HK06-0AB0 from V6.0 all Yes
CPU 414-5H PN/DP 6ES7414-5HM06-0AB0 from V6.0 all Yes
CPU 416-5H PN/DP 6ES7416-5HS06-0AB0 from V6.0 all Yes
CPU 417-5H PN/DP 6ES7417-5HT06-0AB0 from V6.0 all Yes
CPU 1211C 6ES7211-1AD30-0XB0 from V1.02 all, except:
20, 21, 25, 80 102, 123, 5001, 34962, 34963 and 32964
No
6ES7211-1AE31-0XB0 from V3.0
6ES7211-1AE40-0XB0 from V4.0
6ES7211-1BD30-0XB0 from V1.02
6ES7211-1BE31-0XB0 from V3.0
6ES7211-1BE40-0XB0 from V4.0
6ES7211-1HD30-0XB0 from V1.02
6ES7211-1HE31-0XB0 from V3.0
6ES7211-1HE40-0XB0 from V4.0
CPU 1212C 6ES7212-1AD30-0XB0 from V1.02 all, except:
20, 21, 25, 80 102, 123, 5001, 34962, 34963 and 32964
No
6ES7212-1AE31-0XB0 from V3.0
6ES7212-1AE40-0XB0 from V4.0
6ES7212-1BD30-0XB0 from V1.02
6ES7212-1BE31-0XB0 from V3.0
6ES7212-1BE40-0XB0 from V4.0
6ES7212-1HD30-0XB0 from V1.02
6ES7212-1HE31-0XB0 from V3.0
6ES7212-1HE40-0XB0 from V4.0
CPU 1214C 6ES7214-1AE30-0XB0 from V1.02 all, except:
20, 21, 25, 80 102, 123, 5001, 34962, 34963 and 32964
No
6ES7214-1AG31-0XB0 from V3.0
6ES7214-1AG40-0XB0 from V4.0
6ES7214-1BE30-0XB0 from V1.02
6ES7214-1BG31-0XB0 from V3.0
6ES7214-1BG40-0XB0 from V4.0
6ES7214-1HE30-0XB0 from V1.02
6ES7214-1HG31-0XB0 from V3.0
6ES7214-1HG40-0XB0 from V4.0
CPU 1215C 6ES7215-1AG31-0XB0 from V3.0 all, except:
20, 21, 25, 80 102, 123, 5001, 34962, 34963 and 32964
No
6ES7215-1AG40-0XB0 from V4.0
6ES7215-1BG31-0XB0 from V3.0
6ES7215-1BG40-0XB0 from V4.0
6ES7215-1HG31-0XB0 from V3.0
6ES7215-1HG40-0XB0 from V4.0
CPU 1217C 6ES7217-1AG40-0XB0 from V4.0 all, except:
20, 21, 25, 80 102, 123, 5001, 34962, 34963 and 32964
No
Table 01

If you use the SIMATIC CPU as Modbus client, then there are no restrictions regarding the released port numbers. You can set any remote port of the CPU.

Number of possible communication connections using Modbus/TCP protocol
The maximum number of Modbus clients that can be connected to one S7-300 or S7-400 CPU with integrated PROFINET interface is limited by the CPU-specific quantity frameworks. If the CPU with integrated PROFINET interface does not support multiple ports, each local port of the CPU can only be used once, which means that when a communication connection has been established for a local port of the CPU, then you cannot set up another connection through that port.
If a non-multiport CPU is used as Modbus server, then there are two options for establishing communication connections to multiple Modbus clients.

  • You parameterize different port numbers for the Modbus server in the Modbus client.


Bild 01

  • All Modbus clients access the Modbus server through Port 502.
    In this case, it is necessary to have constant job-controlled establishment and clear-down of connections. The Modbus server can communicate with only 1 Modbus client through Port 502 at any one time. The connection to the first Modbus client must be cleared down and Port 502 released before another Modbus client can access the Modbus server. As soon as Port 502 is released, another Modbus client can access the Modbus server via that port.

Case 01

Bild 02

Case 02

Bild 03


Bild 04


Bild 05

Further Information
More information about multiport-compatibility is available in the technical data of the CPU.
If the CPU supports multiple passive connections per port for open IE communication, it is multiport-compatible.
  
Manual Entry ID
SIMATIC S7-300 CPU 31xC and CPU 31x: Technical data 12996906
SIMATIC Distributed IO ET 200S Interface Module IM151-8 PN/DP CPU 47409312
Automation System SIMATIC S7-400 CPU Specifications 53385241
SIMATIC S7-1200 Automation System 36932465
Table 02

 Entry ID:34010717   Date:2014-12-16 
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
Topics
Help
Online Help
Guided Tour