|
Description You can use the FC10 "AG_CNTRL" for connection diagnostics. If required, you can initialize a new connection setup via the FC10.

Fig. 01
The following actions can be executed via parameterizable commands:
- Reading out connection data
Based on the status data of all or individual IE CP connections you can decide whether or not it is useful to reset the connections.
- Resetting configured connections
You can reset individual or all the connections of an IE CP.
The FC10 "AG_CNTRL" commands are permissible for open communication services only with the following protocols:
ISO Transport, ISO-on-TCP (RFC 1006), TCP and UDP.
More information on the FC10 "AG_CNTRL" commands is available in the manual "Functions (FC) and Function Blocks (FB) for SIMATIC NET S7-CPs Programming Manual" in Entry ID 30564821.
The following commands for connection setup and clear-down are not supported by all IE CPs:
| Command |
Description |
CMD 6
"CN_DISCON" |
connection disconnect:
This command resets the connection which has been selected with ID and LADDR. The resetting of the connection is prompted by a connection abort. Any data saved in the stack is lost without notice. The connection is then not established automatically. The connection can be re-established using the "CON_STARTCON" control command. An entry is generated in the diagnostics buffer from which you can read the result of the command. |
CMD 7
"CN_STARTCON" |
start connection:
This command establishes a connection which has been selected with ID and LADDR and which has been aborted beforehand with the control command "CON_DISCON". An entry is generated in the diagnostics buffer from which you can read the result of the command. |
Table 01
The following overview contains information about which commands are implemented on the IE CPs which support the FC10 "AG_CNTRL".
| CMD |
Type |
order no. |
As of firmware version |
| 0-5 |
CP343-1 Lean |
6GK7343-1CX10-0XE0 |
2.1 |
| 0-5 |
CP343-1 |
6GK7343-1EX21-0XE0 |
1.0.17 |
| 0-5 |
CP343-1 |
6GK7343-1EX30-0XE0 |
2.0.16 |
| 0-5 |
CP343-1 Advanced |
6GK7343-1GX21-0XE0 |
1.0.24 |
| 0-5 |
CP443-1 Advanced |
6GK7443-1EX40-0XE0 |
2.2.35 |
| 0-5 |
CP443-1 Advanced |
6GK7443-1EX41-0XE0 |
1.0.24 |
| 0-7 |
CP343-1 Lean |
6GK7343-1CX10-0XE0 |
2.2 |
| 0-7 |
CP343-1 |
6GK7343-1EX30-0XE0 |
2.2 |
| 0-7 |
CP343-1 Advanced |
6GK7343-1GX30-0XE0 |
1.0.23 |
| 0-7 |
CP343-1 Advanced |
6GK7343-1GX31-0XE0 |
3.0 |
| 0-7 |
CP443-1 |
6GK7443-1EX20-0XE0 |
1.0.26 |
| 0-7 |
CP443-1 |
6GK7443-1EX30-0XE0 |
3.0 |
| 0-7 |
CP443-1 Advanced |
6GK7443-1GX20-0XE0 |
2.0 |
| 0-7 |
CP443-1 Advanced |
6GK7443-1GX30-0XE0 |
3.0 |
Table 02
|