Instructions: If you are using the Apple Macintosh operating system Mac-OSX and LOGO! Soft Comfort V6.0 cannot communicate with your LOGO! basic module via the LOGO! USB PC cable, then check whether the /var/lock folder is in your file system. If not, create this folder and make sure that you have complete access rights for it. If, beforehand, you have used a previous version of the RXRXComm package, then you might have to delete any remaining lock files in the previous folder /var/spool/uucp. Check these folders before running the setup application.
Notes:
- In Mac-OSX, you reach the /var folder via the finder menu bar "Go to" -> "Go to folder ...". Under "Open the following folder:" you enter "var" and click on "Open".
If problems arise with access rights, you can set them via the finder menu item "Information" ("Apple" key + "I").
- The current LOGO! Soft Comfort USB PC cable driver for Windows and Linux is available at the following link:
http://www.automation.siemens.com/logo/html_00/support/01ToolsDownloads/index.html
Download: The current LOGO! Soft Comfort USB PC cable drivers for Macintosh are available here to download.
LOGO_USB_PC_Cable_driver_Mac ( 265 KB )
|