show the entry list
S7-300 CPU 31x -- Configuring and programming communication -- Configuring PROFINETinterfaces
How do you display the diagnostics buffer of a SIMATIC CPU with integrated web server on a SIMATIC Panel?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
How do you reset the IP address and device name of an I device?
Why is the message "This page is not available" displayed in the web browser when you call the HTML page "Topology", for example, to read out the topology via the web server of the CPU?
How do you activate the "Prioritized OCM communication" function to improve the OP communication performance?
What should you watch out for when parameterizing the watchdog time when a ring redundancy is established with the Media Redundancy Protocol?
Which CPU can you operate as a PROFINET I device?
What should you watch out for with a remote access to a SIMATIC S7 with STEP 7 via the Internet?
In the user program of an S7-300 or S7-400 CPU with integrated PN interface, how can you read out the current topology of the PROFINET IO system connected?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via Industrial Ethernet in the SIMATIC NET Quick Start Collection?
What differences are there when configuring S7 connections?
Which settings are required to access the web server of the CPU via a PC with a second network card even though a proxy server is set?
Can you implement an S7 317-2 PN/DP CPU instead of an S7 315-2 PN/DP CPU configured in iMap?
How do you read data consistently from a DP standard slave/PROFINET IO device and write it consistently to a DP standard slave/PROFINET IO device?
What can you do when communication errors occur sporadically with a PROFINET interface of the S7 300 CPU 31x-2 PN/DP?
From which library should you take the communications FBs?
What are the commonalities and differences between configured communication connections and the open Ethernet communication?
What are the differences when assigning the MAC address?
S7-400 CPU 41x -- Configuring and programming communication -- Configuring the PROFINET interface
Why is the "Certificate error" message shown in the address line when downloading the web page of an S7-300/400/1200 CPU over "https://..."?
How do you display the diagnostics buffer of a SIMATIC CPU with integrated web server on a SIMATIC Panel?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Why is the message "This page is not available" displayed in the web browser when you call the HTML page "Topology", for example, to read out the topology via the web server of the CPU?
How do you reset the IP address and device name of an I device?
What should you watch out for when parameterizing the watchdog time when a ring redundancy is established with the Media Redundancy Protocol?
Which CPU can you operate as a PROFINET I device?
What should you watch out for with a remote access to a SIMATIC S7 with STEP 7 via the Internet?
In the user program of an S7-300 or S7-400 CPU with integrated PN interface, how can you read out the current topology of the PROFINET IO system connected?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find sample S7 programs and documentation for communication via Industrial Ethernet in the SIMATIC NET Quick Start Collection?
Which settings are required to access the web server of the CPU via a PC with a second network card even though a proxy server is set?
What differences are there when configuring S7 connections?
How do you read data consistently from a DP standard slave/PROFINET IO device and write it consistently to a DP standard slave/PROFINET IO device?
Which settings are required to access the web server of the CPU via a PC with a second network card even though a proxy server is set?
Part number:

Background:
CPUs with the name extension "PN/DP" have a web server. Here, you can read out data from the CPU via the Ethernet using the web browser.

The information in this entry is based on the following scenario:
You are using a computer with two network cards. The first card is connected with the company intranet and the second with the network in which the CPU is located. The company intranet is connected with the Internet only via a proxy server. A proxy server acts as a broker between the internal network (intranet) and the Internet, which calls the files from the remote web server and makes them available.

If you now enter the CPU's IP address in the browser, the request is sent to the proxy server and not to the CPU. Thus you cannot set up a connection with the CPU.

Solution:
Make one of the two settings to access the CPU despite proxy server:

More information:
More information on this is available in Entry ID: 2073614 "What is the connection between subnet masks and IP addresses in the IP address area, also with regard to subnetting?".
Instructions for using the web server are available in Entry ID: 12996906 section 3.3 Web Server.

Use private IP address
Since the area of the private IP addresses is usually not routed in the Internet, the web browser bypasses the proxy server and queries the private (or local) address directly. Therefore, you use private (or local) addresses for the network in which the CPU is located.

Set a private IP address for the CPU (e.g. 192.168.0.4).


Fig. 01

Set a private IP address for the network card (e.g. 192.168.0.2). The CPU and network card must be in the same network.


Fig. 02

In this example, the CPU is accessible via the web browser at http://192.168.0.4/.

The following ranges are reserved for private networks:

10.0.0.0 - 10.255.255.255
172.16.0.0 - 172.31.255.255
192.168.0.0 - 192.168.255.255

Exception for proxy server
If you cannot use a private (or local) IP address, you must inform the browser that this address should be accessed directly without proxy.

Enter the CPU's IP address as exception of the proxy server in the PC's web browser. You find the settings in the Internet Explorer under Tools -> Internet Options -> Connections -> LAN Settings -> Proxy Server -> Advanced.

In this example, the CPU is accessible via the (non-private) IP address http://140.0.0.4/. In this example, the IP address is 140.0.0.2 (CPU and network card must be in the same network).

 
Fig. 03

You can also use wildcards, e.g. "140.0.0.*".

In this example, the CPU is accessible via the web browser at http://140.0.0.4/.

 Entry ID:33269452   Date:2008-12-29 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour