show the entry list

Basic Panels -- Setting up and parameterizing hardware -- Setting up connections  
How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet? 
What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU? 
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project? 
How do you integrate an HMI operator panel into a local network? 
What transfer options are available in the various operator panels? 
When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel? 
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)? 
How can you visualize the current status of the CPU on a WinCC flexible operator panel? 
How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel? 
How do you use WinCC flexible to transfer a project to an operator panel via S7 routing? 

How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet?Go to beginning
Part number:

Description
The document below informs you how to transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet.

Contents

1.Transfer from a Configuration Computer with Windows 7 using Ethernet
    1.1 Instructions
    1.2 Settings on the Operator Panel
    1.3 Settings on the Configuration Computer
    1.4 Checking the Ethernet Connection
        1.4.1 Checking the Connection to the Panel
        1.4.2 Checking the Settings on the Operator Panel
    1.5 Settings in WinCC (TIA Portal)

Download
WinCC_TIA_Portal_Ethernet_Transfer_en.pdf ( 802 KB )

Note on security
Caution
The functions and solutions described in this article confine themselves predominantly to the realization of the automation task. Furthermore, please take into account that corresponding protective measures have to be taken in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the internet. More information can be found in Entry ID: 50203404.

Additional Keywords
Download, Transfer, Load, Control Panel, Channel, Remote Control, Commissioning, Project transfer, Bus address, Transmission rate, Nodes, Stations

What should you watch out for when connecting a SIMATIC HMI device configured with WinCC flexible ES to a SIMATIC ET 200 CPU?Go to beginning
Part number:

Configuration Notes
Please note the following points if you wish to connect a SIMATIC HMI operator panel to an ET 200-CPU.

Properties of the ET 200-CPUs

  • ET 200S CPU
    The IM151-7 CPUs of ET 200S have an MPI/ DP interface.
    In the MPI subnetwork you can use the HMI operator panel to operate the ET 200S CPU via the integrated MPI interface.
    On the PROFIBUS DP the integrated DP interface of the ET 200S CPU can only be used as a DP slave. This means that in addition to the HMI operator panel you need a DP master (S7-300 CPU316-2DP, for example) that operates the IM 151-7 CPU as a DP slave.

    If the IM151-7 CPU is operated without DP master on the PROFIBUS DP, communication with the HMI operator works, but a bus error is displayed on the IM151-7 CPU.

    Note
    With the DP master module (order number 6ES7138-4HA00-0AB0), which you slot directly next to the ET 200S CPU, you can add a DP interface to the ET 200S, which is configured as DP master. With this master interface module it is then possible to operate the ET 200S without any other DP master on the PROFIBUS DP.

    Requirements
    In order to be able to use the DP interface on the master interface module you require a CPU, order number 6ES7151-7AA10-0AB0, and firmware version V2.1 or higher.

  • ET 200X CPU
    The BM147-1 CPUs of ET 200X have an MPI/ DP interface.
    In the MPI subnetwork you can use the HMI operator panel to operate the ET 200X CPU via the interface parameterized as MPI.
    On the PROFIBUS-DP the ET 200X CPU (BM 147-1) can only be used as a DP slave. This means that in addition to the HMI operator panel you need a DP master (S7-300 CPU316-2DP, for example) that operates the BM 147-1 as a DP slave.

    The BM147-2 CPUs of ET 200X have an MPI/ DP interface that can be parameterized as MPI or as a DP slave, and another DP master interface.
    In the MPI subnetwork you can use an HMI operator panel to operate the ET 200X CPU via the interface parameterized as MPI.
    On the PROFIBUS DP the ET 200X CPU BM 147-2 can operate on the one hand as a DP slave with an additional DP master (an S7-300 CPU 315-2DP, for example). On the other hand the BM147-2 CPU can also communicate as DP master with the HMI operator panel via the DP master interface.

Warning
The ET 200 CPU is configured in the SIMATIC Manager in a
SIMATIC S7-300 station.

Options for connecting an HMI operator panel to the ET 200 CPUs

Connecting the HMI operator panel via MPI to the ET 200 CPU
You can connect the HMI operator panel via MPI directly to an IM151 CPU or BM147 CPU.


Fig. 01

Setting in the STEP 7 Hardware Configuration
In the Properties dialog of the MPI/DP interface of the ET 200 CPU you set the type of interface to MPI and then connect the station to the MPI subnetwork.


Fig. 02

Settings in the STEP 7 Hardware Configuration of the SIMATIC HMI station
Double-click the HMI MPI/DP interface of the HMI station and network it with the ET 200 CPU via MPI.


Fig. 03

Enabling the connection in WinCC flexible ES
Open the HMI station with WinCC flexible ES. Under Communication > Connections you enable the connection already created to the ET 200 CPU.

Note
The "Cyclic operation" option must be deselected.


Fig. 04

Connecting the HMI operator panel via PROFIBUS DP to the ET 200 CPU

  1. Version: CPU 316-2DP as DP master, ET200 CPU as DP slave
  2. Version: ET200S CPU with DP master module
  1. Version: CPU 316-2DP as DP master, ET200 CPU as DP slave

The ET 200 CPU is operated as DP slave on the PROFIBUS DP subnetwork. This means that in addition to the HMI operator panel and the ET 200 CPU (IM151 CPU or BM147 CPU) you need a DP master (S7-300 CPU 316-2DP, for example) on the PROFIBUS DP subnetwork.


Fig. 05

Settings in the STEP 7 Hardware Configuration of the ET 200 CPU for supporting ALARM_S messages
In order for the ET 200 CPU to support the ALARM_S service, in the Properties of the DP interface of the IM151 CPU or BM147 CPU under Operating Mode you must enable the option Test, commissioning, routing.


Fig. 06

Settings in the STEP 7 Hardware Configuration of the S7-300 DP master
Once you have networked the ET 200 CPU with PROFIBUS DP, open the Hardware Configuration of the DP master station (CPU 316-2DP) and there you configure the ET 200 CPU as a DP slave.


Fig. 07

Settings in the STEP 7 Hardware Configuration of the SIMATIC HMI station
Double-click the HMI MPI/DP interface of the HMI station and network it with the ET 200 CPU via PROFIBUS.


Fig. 08

Enabling the connection in WinCC flexible ES
Open the HMI station with WinCC flexible ES. Under Communication > Connections you enable the connection already created to the ET 200 CPU.

Note
The "Cyclic operation" option must be deselected.


Fig. 09  

  1. Version: ET200S CPU with DP master module

The ET 200S is operated with the DP master interface module as DP master on the PROFIBUS DP. The HMI operator panel is connected to the master module via PROFIBUS.


Fig. 10

Settings in the STEP 7 Hardware Configuration
Network the DP master module of the ET 200S with a newly created PROFIBUS network.
The master interface module is located in the Hardware Catalog in the project tree from which you configured the IM151-7 CPU.


Fig. 11

Settings in the STEP 7 Hardware Configuration of the SIMATIC HMI station
Double-click the HMI MPI/DP interface of the HMI station and network it with the DP master module of the ET 200 CPU via PROFIBUS.


Fig. 12

Enabling the connection in WinCC flexible ES
Open the HMI station with WinCC flexible ES. Under Communication > Connections you enable the connection already created to the ET 200 CPU.

Note
The "Cyclic operation" option must be deselected.


Fig. 13

Connecting the HMI operator panel (MPI) via routing (CPU 316-2DP: DP Master) to the ET 200-CPU (DP-Slave)
THe ET 200 CPU (IM151 CPU or BM147 CPU) is operated as a DP slave on an S7-300 CPU 316-2DP (DP master). The HMI operator panel is connected to the S7-300 via MPI. Via routing (MPI <-> PROFIBUS DP) a connection is set up between the HMI operator panel and the ET 200 CPU.


Fig. 14

Settings in the STEP 7 Hardware Configuration of the ET 200 CPU for supporting ALARM_S messages
In order for the ET 200 CPU to support the ALARM_S service, in the Properties of the DP interface of the IM151 CPU or BM147 CPU under Operating Mode you must enable the option Test, commissioning, routing.


Fig. 15

Settings in the STEP 7 Hardware Configuration
Once you have networked the ET 200 CPU with PROFIBUS DP, open the Hardware Configuration of the DP master station (CPU 316-2DP) and there you configure the ET 200 CPU as a DP slave. The S7-300 station must also be networked with MPI.

 
Fig. 16

Settings in the STEP 7 Hardware Configuration of the SIMATIC HMI station
Double-click the HMI MPI/DP interface of the HMI station and network it with the DP master module of the S7 -300 CPU (CPU 316-2DP) via MPI.


Fig. 17

Enabling the connection in WinCC flexible ES
Open the HMI station with WinCC flexible ES. Under Communication > Connections you enable the connection already created to the ET 200 CPU.

Note
The "Cyclic operation" option must be deselected.


Fig. 18

Overview: HMI operator panels with ET 200 CPU
 

HMI operator panel

Communication
HMI operator panel
with
ET 200-CPU

Alarm_S messages supported

ProAgent
options package supported
KTP400 Basic - - -
KTP600 Basic X1) - -
KTP1000 Basic X1) - -
TP1500 Basic - - -
OP 73micro - - -
TP 170micro - - -
TP 177micro - - -
OP 77A X - -
OP 77B X X -
TP 170A X - -
TP 177A X - -
TP 170B X X -
TP 177B X X -
TP 177B 4" X X -
OP 170B X X -
OP 177B X X -
Mobile Panel 170 X X -
Mobile Panel 177 X X -
TP 270  X X X
TP 277  X X X
OP 270 X X X
OP 277 X X X
MP 177 X X X
MP 270 X X X
MP 270B X X X
MP 277 X X X
Mobile Panel 277 X X X
Mobile Panel 277 IWLAN - X X
Mobile Panel 277F IWLAN - X X
MP 370 X X X
MP 377 X X X
ProTool/Pro RT X X X
WinCC flexible RT X X X
1) Applies only for the DP version of this operator panel

Note
More information on configuring Alarm_S messages and the display on the operator panel is available in the Support Shop in Entry ID: 24013249.

How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?Go to beginning
Part number:

Description
This entry includes the error messages of a frequency converter in the form of a text list. This enables you to display the error messages in plain text on the operator panel.
Information about using text lists is available at the links below.

  • Manual WinCC (TIA Portal): "WinCC Advanced > Visualize processes (Advanced) Configuration > Working with text lists and graphics lists > Working with text lists"
  • Manual WinCC flexible: ""WinCC flexible 2008 > "WinCC flexible Engineering System > Working with WinCC flexible > Text lists"

The tables below provide the error messages as libraries that can be downloaded.

1. Downloads for WinCC (TIA Portal)
 
Firmware SINAMICS S110 SINAMICS S120 SINAMICS G110 SINAMICS G120
V 2.5 SP1
HF3
  ( 709 KB )    
V 2.6 SP1   ( 730 KB )    
V 3.0     ( 484 KB ) ( 484 KB )
V 3.2     ( 488 KB ) ( 486 KB )
V 4.3 ( 638 KB ) ( 638 KB )

 

( 638 KB )
V 4.4 ( 737 KB ) ( 737 KB )   ( 737 KB )
MICROMASTER SINAMICS DCM
( 484 KB ) ( 483 KB )

2. Downloads for WinCC flexible
 
Firmware SINAMICS S110 SINAMICS S120 SINAMICS G110 SINAMICS G120
V 2.5 SP1
HF3
 

( 6466 KB )

   
V 2.6 SP1  

( 6595 KB )

   
V 3.0    

( 3543 KB )

( 3354 KB )
V 3.2    

( 3388 KB )

( 3357 KB )
V 4.3 ( 5597 KB )

( 5352 KB )

 

( 5524 KB )
V 4.4 ( 6988 KB ) ( 5794 KB )   ( 6972 KB )
MICROMASTER SINAMICS DCM
( 3464 KB ) ( 1015 KB )

The libraries are available for downloading in WinCC flexible versions 2007, 2008 and 2008 SP2. If you want to use the libraries in older versions of WinCC flexible too, you must save them in the version concerned in each case. More information about this is available in Entry ID: 33934262.

Note
The libraries are available in German, English (GB and US), French, Spanish, Italian and Chinese.
Define the language you wish to have prior to inserting the library:

  • In WinCC flexible under "Language Settings > Project Languages"

  • In WinCC (TIA Portal) under "Languages & Resources > Project languages"

Additional Information
More related information is available in the Online Support at the links below.
 
Product Direct connection
HMI/Frequency converter
Frequency converter
Error lists for HMI
WinCC (TIA Portal) 58522638 This entry
WinCC flexible 29522676

Note on security
The functions and solutions described in this article confine themselves predominantly to the realization of the automation task. Furthermore, please take into account that corresponding protective measures have to be taken in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the internet. More information can be found in Entry ID: 50203404.

How do you integrate an HMI operator panel into a local network?Go to beginning
Part number:

Instructions
The example below explains how to

  1. Incorporate an operator panel into a local network in order to back up a tag archive to a PC via the local network.
  2. Share a folder or a drive on a PC.
  3. Save a tag archive to a PC via a local network.

Note
This entry uses a simple example to explain how to integrate an operator panel into a network. Other network constellations are also possible, but these generally require further knowledge of networks.

Attachment 1: Procedure for WinCC(TIA Portal) and Windows 7 ( 1128 KB )

Contents
1 Setting Up a Network Connection
    1.1 Assigning a Fixed IP Address in Microsoft Windows XP
    1.2 Network Configuration on the Operator Panel
    1.3 Additional Settings on the PC
    1.4 Testing the Network Connections
2 Enabling Sharing
3 Saving the Tag Archive

Attachment 2: Procedure for WinCC flexible and Windows XP ( 1139 KB )

Note
For activating a printer over the network, for example, (see Entry ID: 18720136) addressing must also take place through a "name resolution".

Additional Keywords
GMP, Pharma, Life Science, Validation, FDA 21 CFR Part 11

What transfer options are available in the various operator panels?Go to beginning
Part number:

Transfer options
Attachment 1 lists the operator panels and their transfer options.

Attachment 1: Projecttransfer_V1_2_e.pdf ( 17 KB )    

USB host-to-host cables
More information on the topic of "USB host-to-host cables" is available in Entry ID: 19142034.

Application of adapters and cables
Attachment 2 indicates for each operator panel the plug-in cable required for the following applications:

  • Process coupling
  • Download (update operating system, project, ...)
  • Booting (filling in the case of a missing or damaged operating system)

Attachment 2: Panels_connecting_cables_V1_2_e.pdf ( 29 KB )  

Notes on USB PC adapter (6ES7972-0CB20-0XA0)and USB A2 PC adapter (6GK1 571-0BA00-0AA0)
The USB PC adapter/USB A2 PC adapter provides an MPI/DP interface through the PC's USB interface. More information about the USB PC adapter is available in the manual in Entry ID: 16983464 More information about the USB A2 PC adapter is available in the manual in Entry ID: 68849363
These cables are released only for the devices below for project transfer and OS updating.

  • OP 73
  • OP 77 A
  • TP 177 A
  • KTP600 Basic Color DP
  • KTP1000 Basic Color DP

Using USB RS232 adapters and USB Ethernet adapters
When using the RS232/PPI Multi-Master cable, zero modem cable or Ethernet connections, you can only use the "real" interfaces for project transfer.
"Real" interfaces are interfaces without implementation via USB. This means that you cannot use any "USB to serial" or "USB to Ethernet" adapters.

Additional Keywords
Project transfer, Project download, WinCC flexible, Transfer cable, ProTool, RS 232, PC/PPI cable, PC PPI cable, RS 485, Com Text, Cables, USB adapter

When using the "Kaspersky" virus scanner, why does the WinCC flexible configuration PC crash after transfer to an operator panel?Go to beginning
Part number:

Description:
After project transfer to an operator panel, the configuration PC crashes or no longer works reliably.
This behavior can be caused by using the "Kaspersky" virus scanner. It occurs as from version V6.0. The crash is due to a security update from "Kaspersky".

Remedy:
The "Kaspersky" virus scanner is not released for WinCC flexible. You can remedy this behavior as follows.

  1. Uninstall or deactivate the "Kaspersky" virus scanner.
  2. Release the processes "Hmies.exe" and "TransferTool.exe" in the virus scanner.

Note:
More information on the topic of "Virus scanners with WinCC flexible" and on the compatibility of tested virus scanners is available in the WinCC flexible help system under:
 "First Steps > Installation Guide > Installation > Installing WinCC Flexible > Antivirus tools".

How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?Go to beginning
Part number:

Description
This entry describes how to establish a direct connection between HMI Panels and frequency converters.

Please follow the instructions in the PDF file.

  direct_connection_HMI_frequency_converter_e.pdf ( 1584 KB )

Note
The SINAMICS G120 Control Units CU230P-2, CU240B-2 and CU240E-2 do not support the function described.

Additional Information
More related information is available in the Online Support at the links below.
 
Product Direct connection
HMI/Frequency converter
Frequency converter
Error lists for HMI
WinCC (TIA Portal) 58522638 47520881
WinCC flexible This entry

Note on security
The functions and solutions described in this article confine themselves predominantly to the realization of the automation task. Furthermore, please take into account that corresponding protective measures have to be taken in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the internet. More information can be found in Entry ID: 50203404.

How can you visualize the current status of the CPU on a WinCC flexible operator panel?Go to beginning
Part number:

This FAQ describes how to visualize the current status of a CPU and have it displayed reliably on a panel.

Please follow the instructions in the PDF file.

Attachment: CPU_Status_anzeigen_e.pdf ( 1066 KB )

Sample program:

1. Complete evaluation of the CPU status:

Attachment: CPU_Status_anzeigen.zip ( 6035 KB )
 
Components Product and version designation
HMI software WinCC flexible 2008 SP1
HMI Panel PC Runtime
CPU S7 300 CPU / S7 400 CPU
Software STEP 7 V5.4 SP2
 

2. Evaluate connection status without alarm display:

Attachment: CPU_Status_anzeigen_SP1.zip ( 1871 KB )
 
Components Product and version designation
HMI software WinCC flexible 2008 SP1
HMI Panel PC Runtime
CPU S7300 / S7400

Runnability and test environment:
The tables above list the components that have been used to create this entry and verify the functions described.

Keywords:
Life bit monitoring, Communication monitoring, Connection monitoring, Connection status, PLC connection interrupted, Stop, Run

How can you have any number of automation systems addressed one after the other by the "Change Connection" function with WinCC flexible PC Runtime or a Panel?Go to beginning
Part number:

This FAQ describes how to use the "Change Connection" function to address multiple controllers with just one configured connection. This FAQ covers all panels and the PC Runtime.

Please follow the instructions in the PDF file.

Attachment: 35508221_change_connection_e.pdf ( 1267 KB )

Sample program:

Attachment: 35508221_project_change_connection.zip ( 2281 KB )

Runnability and test environment:
The following table lists the components that have been used to create this entry and verify the functions described.
Components Product and version designation
HMI software WinCC flexible 2008 SP1
HMI Panel PC Runtime
CPU S7 300 CPU / S7 400 CPU

Note on using direct keys
The WinCC flexible function "Change Connection" does not change the connection of direct keys.

How do you use WinCC flexible to transfer a project to an operator panel via S7 routing?Go to beginning
Part number:

Contents

Introduction
Notes and requirements for S7 Routing
S7 Routing example
Procedure for transfer via S7 Routing  

Introduction for S7 Routing
You can load an HMI project from a WinCC flexible configuration computer to an operator panel over different subnets.
If you implement a router, you can establish a connection between different subnets. A SIMATIC station can act as a router if it has suitable interfaces.
The modules with communications capability (CPUs or CPs), which create gateways between the subnets, must support routing.
To transfer a WinCC flexible project, the WinCC flexible configuration computer must be connected to an MPI bus, PROFIBUS or Ethernet.
The operator panel to which the WinCC flexible project is to be transferred must also be connected to an MPI bus, PROFIBUS or Ethernet.

Notes and requirements for S7 Routing

Notes

  • Refer to a component's technical documentation to establish whether it supports routing.
    Alternatively, open the component's object properties in NetPro or in HW Config. The "General" tab contains a brief description of the properties.
    Information about which modules possess routing capability is also available in Entry ID: 584459.
  • The requirements that have to be fulfilled to perform STEP 7 routing by means of a PG/PC station are given in Entry ID: 16620173.
  • A routing connection for the transfer can also be established by means of multiple routing partners. Routing cannot be used as a means of transferring to PC-based operator panels (PC Runtime) with an activated station manager (Station Configuration Editor).
  • In order to establish a routing connection, all the stations within a STEP 7 project must be configured and loaded.
  • You must use NetPro to configure all the devices and subnets connected to the network.

S7 Routing MPI / PROFIBUS and Ethernet
Below is a list of the requirements and the supported HMI operator panels and the possible routes for S7 Routing are shown in Fig. 01.

  • At least WinCC flexible 2005
  • At least STEP 7 V5.3 SP2
  • All panels including PC Runtime except PC Station with Station Configuration Editor


Fig. 01

S7 Routing Ethernet with WinCC flexible 2008
The S7 Routing function was extended with WinCC flexible 2008. Below is a list of the requirements and the supported HMI operator panels and the possible routes for S7 Routing are shown in Fig. 02.

  • At least WinCC flexible 2008
  • At least STEP 7 V5.4 SP3
  • You can use only the following devices for routing over the "S7 Ethernet" transfer channel:
    • TP 177B 4"
    • MP 177
    • Mobile Panel 277
    • MP 277
    • MP 377
  • Routing over Ethernet is not possible with WinCC flexible PC Runtime.
  • In the case of routing by way of SIMOTION CPU 4.1.2, transfer of the configuration over S7 Ethernet does not work.
  • Routing from MPI/DP to Ethernet is possible if MPI/DP has been selected in the Transfer settings.


Fig. 02

S7 Routing Ethernet and WinCC flexible 2008 SP3
More devices were added to the S7 Routing function with WinCC flexible 2008 SP3.
Below is a list of the requirements and the supported HMI operator panels and the possible routes for S7 Routing are shown in Fig. 03.

  • At least WinCC flexible 2008 SP3
  • At least STEP 7 V5.4 SP3
  • You can also use the following devices for routing over the "S7 Ethernet" transfer channel:
    • OP 77B
    • OP 177B
    • TP 177B
    • Mobile Panel 177
    • OP 277
    • TP 277 


Fig. 03

Download
The download below includes a summary of the possible routes for S7 Routing and their requirements.

WinCC_flexible_Routing.pdf ( 56 KB )

Example of S7 Routing with Ethernet
Fig. 01 shows a routing connection between the WinCC flexible configuration computer (network object: Stations > PG/PC) and operator panel "MP 377 15'' Touch" (network object): Stations > SIMATIC HMI station). The "SIMATIC 300(1)" programmable logic controller acts as a router.

Use NetPro to configure the routing connection between the devices involved.
You must assign the interface of the configuration computer. You can recognize the assignment by the yellow connection line to the subnet and by the yellow arrow in the station symbol.

The procedure for configuring a routing connection is described in Entry ID: 2383206.


Fig. 04

Procedure for transfer by means of S7 routing

  1. Open the HMI station in WinCC flexible.
  2. Select the menu command "Project > Transfer > Transfer Settings".
  3. Select the operator panel.
  4. Select the mode and check the "Enable routing" option box.
    The mode must match the communication channel.
  5. In the "Next station" box, you select the bus type of the next and the last connection.
    The network addresses of the next routing partner and destination device are displayed.
    Any routing partners positioned between them are not displayed here.
  6. Transfer your project by clicking the "Transfer" button.


Fig. 05: Transfer settings for MPI/PROFIBUS


Fig. 06: Transfer settings for Ethernet

More information in manual
More information on the topic of "Project transfer via S7 Routing" is available in the WinCC flexible manual in Entry ID: 18796010.

 

 Entry ID:33087853   Date:2013-05-03 
I regard this article....as helpfulas not helpful                                 






























related links
SIMATIC HMI WinCC flexible 2008 W ...
Communications between SIMATIC ET ...
SIMOTION Documentation Package fo ...
STEP 7 Professional V11.0 SP1
STEP 7 Basic V11.0 SP1
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour