Description: Use the SIMATIC ET 200 Selection Tool to configure your ET 200S station. This configuration tool guides you simply and easily through the configuration of an ET 200S station and supports you in selecting the various components and matching accessories.
The SIMATIC Selection Tool is in the configuration tool overview of the Industry Mall under Automation Technology.
Industry Mall
More information on the guidelines for configuring an ET 200S station is available in the following entries and in the operating instructions for the ET 200S remote I/O system.
| Topic |
Entry ID |
| What conditions do you have to comply with when configuring ET 200S modules? |
21406019 |
| What should you watch out for regarding the compatibility of I/O modules and interface modules when configuring an ET 200S? |
22407397 |
| F system, combination of fail-safe and non-fail-safe I/O modules in an ET200 station |
14198063 |
| What should you watch out for when using the fail-safe module 4 F-DI/3 F-DO 24V/2A (6ES7 138-4FC00-0AB0) in the central setup with the IM151-7 F-CPU? |
27864355 |
| Configuring and running a fail-safe ET 200S system |
14196395 |
| Which ET 200S modules support the option handling function? |
22564754 |
| Installation guidelines for ET 200S in Explosion Protection Zone 2 |
13702947 |
| Manual "SIMATIC Distributed I/O System ET 200S" |
1144348 |
|