show the entry list
WinCC flexible ES -- Creating HMI configurations -- Synchronizing date and time
What settings are to be made in Windows 7 in order to change the system time of the PC by means of WinCC flexible Runtime/WinCC Runtime Advanced V11?
How can you calculate the actual local time (summer time or winter time) in the S7-300/400 CPU and then use it on the panel as system time?
How do you synchronize the data and time between a SIMATIC HMI panel and a SIMOTION controller?
How do you synchronize date/time between a TP170A / TP170micro / TP177micro and an S7-200 CPU with WinCC flexible?
How do you synchronize the date and time between a TP170A and the S7-300/S7-400 controller with WinCC flexible?
How do you synchronize the date and time between an operator panel and an S7-300/S7-400 controller with WinCC flexible?
How do you synchronize the system clock between a Windows-based panel and an S7-200 CPU with WinCC flexible?
How do you do the summer/winter time switchover with WinCC flexible (update to version V1.1)?
How do you change the date format in WinCC flexible?
WinCC flexible RT -- Setting up systems -- Configuring software
Why is the script shown in bold type in the PC Runtime although it is not configured as bold type?
How can you optimize the picture change times of WinCC flexible Runtime on a PC with Intel graphics chipset?
How do you insert error messages of a frequency converter (SINAMICS and MICROMASTER) in a WinCC flexible or WinCC (TIA Portal) project?
How do you simulate the system keyboard via K or F-keys?
How do you change the date format in WinCC flexible?
How do you temporarily lock multiple operator panels?
How do you use a key switch to lock/activate the call of specific screens?
How do you establish a direct connection between HMI Panels and frequency converters (SINAMICS and Micromaster)?
How do you configure the WinCC Autostart for WinCC flexible Runtime?
Which settings must you make on the RT Loader to transfer a WinCC flexible Runtime file from the configuration computer to a visualization PC?
Mobile Panels -- Creating HMI configurations -- Setting and editing date and time
How do you do the summer/winter time switchover with WinCC flexible (update to version V1.1)?
How do you synchronize the system clock between a Windows-based panel and an S7-200 CPU with WinCC flexible?
How do you synchronize the system clock between a Windows-based panel and an S7-200 CPU with ProTool?
How do you synchronize the date and time between a Windows-based operator panel and the S7-300/S7-400 controller with ProTool?
How do you synchronize the date and time between an operator panel and an S7-300/S7-400 controller with WinCC flexible?
How do you change the date format in WinCC flexible?
Touch Panel / Operator Panel -- Creating HMI configurations -- Setting and editing date and time
How do you do the summer/winter time switchover with WinCC flexible (update to version V1.1)?
How do you synchronize the system clock between a Windows-based panel and an S7-200 CPU with WinCC flexible?
How do you synchronize the system clock between a Windows-based panel and an S7-200 CPU with ProTool?
How do you synchronize date/time between a TP170A / TP170micro / TP177micro and an S7-200 CPU with WinCC flexible?
How do you synchronize the date and time between a TP170A and the S7-300/S7-400 controller with WinCC flexible?
How do you synchronize the date and time between a Windows-based operator panel and the S7-300/S7-400 controller with ProTool?
How do you synchronize the date and time between an operator panel and an S7-300/S7-400 controller with WinCC flexible?
How do you change the date format in WinCC flexible?
Multi Panel -- Creating HMI configurations -- Setting and editing date and time
How do you synchronize the system clock between a Windows-based panel and an S7-200 CPU with WinCC flexible?
How do you synchronize the system clock between a Windows-based panel and an S7-200 CPU with ProTool?
How do you synchronize the date and time between a Windows-based operator panel and the S7-300/S7-400 controller with ProTool?
How do you synchronize the date and time between an operator panel and an S7-300/S7-400 controller with WinCC flexible?
How do you change the date format in WinCC flexible?
How do you change the date format in WinCC flexible?
Part number:

Description:
You can change the date format on a PC via the Windows Control Panel under "Regional and Language Options". On a Windows-based panel, you can change the date format in the Control Panel under "Regional Settings".

Contents:

  1. Changing the date format for WinCC flexible PC Runtime
  2. Changing the date format on a Windows CE Panel

Note:
In Windows, configuration of the date format depends on the language used.

1. Changing the date format for WinCC flexible PC Runtime
 
No. Procedure
1 Open the Control Panel
  • Open the Windows Control Panel.

Windows 2000

  • Click on "Regional Options" in the Control Panel.

Windows XP and Windows Vista

  • Open "Regional and Language Options" in the Control Panel.


Fig. 01

2 Change standards and formats

Windows 2000

  • Click on "Date" tab in Regional Settings of the Control Panel.

Windows XP

  • In the "Regional Options" tab you click on the "Customize..." button.
Windows Vista
  • In the Formats tab you click on the "Change this format..." button.


Fig. 02

3 Change date format

Windows 2000

  • Change the date format under "Short Date".
  • Then click on "OK".

Windows XP and Windows Vista

  • In the new dialog, select the "Date" tab.
  • Change the date format under "Short Date" or "Date Format".
  • Then click on "OK".


Fig. 03

4 Close dialog and Control Panel

Windows 2000

  • Click on "X" to close the Control Panel.

Windows XP and Windows Vista

  • Click "OK" to close the dialog. 
  • Click on "X" to close the Control Panel.
5 Optional - start WinCC flexible
  • Start WinCC flexible ES or a WinCC flexible RT project.


Fig. 04


2. Changing the date format on a Windows CE Panel
 
No. Procedure
1 Open the Control Panel
  • Open the Control Panel on the Windows-based panel
  • Click on "Regional Settings" in the Control Panel.


Fig. 05

2 Change date format
  • In the "Regional and Language Settings" dialog you click on the "Date" tab.
  • Select the desired date format.
  • Click "OK" to close the dialog. 


Fig. 06

3 Close the Control Panel
  • Close the Control Panel with "X".
  • Optional - Start the WinCC flexible Runtime.

Keywords:
Date format, Date formatting, Display of the date, Date view

 Entry ID:32199678   Date:2008-11-17 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour