show the entry list
ET 200S (standard modules) -- Setting up and parameterizing hardware -- Initializing and parameterizing modules
Why is the menu item for starting S7-PCT in STEP 7 disabled in some IO Link master modules?
How can you group together the address area of the ET 200S in STEP 7 (TIA Portal) using the "Pack Addresses" function?
How do you commission the serial interface module 1SI 3964/ASCII (6ES7138-4DF01-0AB0) in STEP 7 Professional V11 and higher?
How do you commission the serial interface module 1SI MODBUS/USS (6ES7138-4DF11-0AB0) in STEP 7 Professional V11 and higher?
Which "local_device_id" do you parameterize in order to establish a connection to FB65 "TCON" for open communication via Industrial Ethernet?
Why is the message "This page is not available" displayed in the web browser when you call the HTML page "Topology", for example, to read out the topology via the web server of the CPU?
How do you reset the IP address and device name of an I device?
Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible?
Where can you find sample S7 programs and documentation for communication via PROFINET on the SIMATIC NET Quick Start Collection?
Where can you find information of the reproducibility of delay interrupts and cyclic interrupts for IM151-8 and IM154-8?
How is reparameterization performed when replacing the IO link master module or the IO link device?
Which options are available for configuring the ET 200 stations?
Where can you find information on installation guidelines for an ET 200S station?
Which diagnostics messages might you get when commissioning the ET 200S as PROFINET IO device?
Which diagnostics messages might you get when commissioning the ET 200S as PROFIBUS DP slave?
TeleService with ET200S (IM151-CPU) and TS Adapter
Can I use a Quickstop function with an ET 200S Motor Starter?
How can you combine fail-safe and standard modules in the ET 200 stations?
Parameterizing ET 200 S DI 4xNAMUR (6ES7 131-4RD00-0AB0)
Temperature compensation of a thermocouple using a resistance thermometer Pt100 to capture the reference junction temperature
Temperature Compensation of a Thermo-element via the Electronic module 2AI TC HF
How can you group the addresses of ET200S IM151-1 HF (pack addresses) in HW Config?
IM 151-7 CPU: Porting Programs with Packed Addresses
How can you group together the address area of the ET 200S (pack addresses)?
Which ET 200S modules support the option handling function?
What conditions do you have to comply with when configuring ET 200S modules?
What should you watch out for regarding the compatibility of I/O modules and interface modules when configuring an ET 200S?
How can you use Bürkert pneumatic modules in the ET 200S remote I/O system?
How can you prevent the bus error LED from lighting on interface module IM 151 when using reserve modules?
Which diagnostics messages might you get when commissioning the ET 200S as PROFINET IO device?
Part number:

Description:
This entry provides you with information on possible diagnostics messages you might get when commissioning an ET 200S as PROFINET IO device.

Proceed as follows to determine the diagnostics message.

  • In the SIMATIC Manager, you open the menu "PLC > Show Accessible Nodes" to diagnose the separate nodes of the PROFINET IO system.
  • Right-click the PROFINET IO device you wish to diagnose and select the menu "PLC -> Module status".
  • The "Module Status" dialog opens.
  • In the "IO Device Diagnostics" tab you see the standard diagnostics message of the PROFINET IO device which you might get during commissioning.

The following standard diagnostics message indicates that there is not termination module slotted in the ET 200S. You also get this standard diagnostics message when more than one module of the ET 200S station has been removed.


Fig. 01: Termination module not slotted or more than one module of the ET 200S station removed

The standard diagnostics message "Module missing..." indicates that a module in the ET 200S has been removed. Check whether a module is slotted in the specified slot in the ET 200S station.


Fig. 02: A module of the ET 200S station removed

The standard diagnostics message "Incorrect module..." indicates that a different module to the one slotted in the ET 200S has been configured. Check in the STEP 7 hardware configuration whether the module you have configured for the slot specified is the one that is slotted in that slot in the ET 200S station.


Fig. 03: Incorrect module configured 

The following table gives you an overview of the STATUS of SF and BF LEDs when you get one of the above-mentioned standard diagnostics messages.
 
Diagnostics message SF BF
Termination module not slotted (when starting up the ET 200S station) Off Flashes
More than one module of the ET 200S station removed Lights continuously Flashes
One module of the ET 200S station removed Lights continuously Off
Incorrect module configured  Lights continuously Off

 Entry ID:32118459   Date:2008-11-06