show the entry list
Box PC -- Setting up systems -- Parameterizing systems
Why is a picture of the SIMATIC IPC not displayed when you access with the SIMATIC IPC Remote Manager by means of AMT?
Which slot do you have to configure when using the WinAC RTX 2010 with WinCC V11?
How can you set up auto logon for SIMATIC IPCs?
Why does the installation of SQL Express 2005 on a SIMATIC IPC with embedded operating system abort?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
How can you change the designation of the LAN interface in Windows so that the identification of the network interfaces matches between housing sticker and Windows (Box PC 627B and Box PC 827B)?
How can you ensure operation of Windows 2000 with hard disks greater than 120 GB?
Deactivation of fan monitoring in the SOM software
Computer crash when opening the diagnostics for the CP5611 in Windows 2000
Restart after installing MS Windows 98SE is not possible
Box PC 620 / Panel PC 670 - after installing a CP 1613 / CP 5611 Microsoft Win 2000 no longer starts or Windows shuts itself down
How can you avoid faults in the graphics display in Windows XP with the Box PC 840 V2?
Rack PC -- Setting up systems -- Configuring systems
Why is a picture of the SIMATIC IPC not displayed when you access with the SIMATIC IPC Remote Manager by means of AMT?
Which slot do you have to configure when using the WinAC RTX 2010 with WinCC V11?
How can you set up auto logon for SIMATIC IPCs?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
How can you ensure operation of Windows 2000 with hard disks greater than 120 GB?
What can you do about the screen display sporadically freezing or the screen resolution switching to VGA mode with the Rack PC 840 V2?
Keyboard lock for WinCC Runtime with SIMATIC Rack PC IL 40 S and IL 40 S V2
Panel PC -- Setting up systems -- Configuring systems
How can you speed up the opening of the "Onscreen Keyboard" with SIMATIC IPC277D?
How do you configure the "Message Buffer Partition" with a SIMATIC IPC?
How do you switch from landscape to portrait format with SIMATIC IPC277D?
Why is a picture of the SIMATIC IPC not displayed when you access with the SIMATIC IPC Remote Manager by means of AMT?
Which slot do you have to configure when using the WinAC RTX 2010 with WinCC V11?
How can you set up auto logon for SIMATIC IPCs?
Why does the installation of SQL Express 2005 on a SIMATIC IPC with embedded operating system abort?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
How can you ensure operation of Windows 2000 with hard disks greater than 120 GB?
How can I log in on a Windows 2000 computer without keyboard (e.g. Panel PC)?
Function "Change Operating Mode" with the parameter "Serial Transfer"
How can you implement Sm@rtAccess (HTTP communication) and Sm@rtServices (HTML pages) on a Panel PC 477B with WinCC flexible RT?
Changing the background lighting, the key code and triggering of function keys on the SIMATIC Panel PC 670/ 870 under WinNT
Restoring the touch functionality on the PC 670 after reinstalling the operating system
Which software tools are available for the SIMATIC Panel PCs 870 with function keys?
Softwaretools for SIMATIC Panel PCs 670 (with function keys)
Difficulties when Shutting Down Windows 98 Second Edition
Displayed Windows View turned by 180 degrees at IL70
Microsoft Windows 9x and memory extension of more than 512 MB
WinCC flexible ES -- Product information -- General information
What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook?
How do you make printouts on different printers in WinCC flexible PC Runtime?
How can you exchange data between USB storage devices on the Thin Client with an active RDP connection?
What are the functional differences between the different SIMATIC panels?
What options are there for creating a screenshot in WinCC flexible ES, WinCC flexible Runtime or on panels?
What support does Siemens AG offer to make products comply with FDA regulations?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
How do you send customer projects to Technical Support?
Why are PDF documents not displayed properly on the MP377?
Which GSD files are there for the Profibus DP operator panels?
Which GSDML files are there for the operator panels for Profinet IO?
Is there a Siemens contact for customer-specific software solutions, extensions to WinCC flexible or own applications for Windows CE Panels?
WinAC RTX -- Product information -- Determining performance and quantity frameworks
What new features do Intel® Atom™ processors have and what advantages do SIMATIC IPCs with Intel® Atom™ processors offer when used with SIMATIC software?
How do you incorporate the execution times of the F blocks for the Mobile Panel 277F IWLAN into the "S7fcotia.xls" table?
Why does the Windows application load increase to 100% after installing WinAC RTX 2008/2009?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
WinAC RTX F -- Product information -- Determining performance and quantity frameworks
What new features do Intel® Atom™ processors have and what advantages do SIMATIC IPCs with Intel® Atom™ processors offer when used with SIMATIC software?
What are the system limits in an F CPU for safe bidirectional data communication via S7 Communication?
Why does the Windows application load increase to 100% after installing WinAC RTX 2008/2009?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
What different CPU technologies are available in the PC sector and what are the advantages offered by SIMATIC PCs with Intel® Core™ 2 Duo processors when using SIMATIC software?
Part number:

Description
The White Paper on the topic of Intel® Core™ 2 Duo with SIMATIC PCs explains various CPU technologies and technical terms. Among other things, it demonstrates the advantages of implementing SIMATIC PCs with Intel® Core™ 2 Duo processors in combination with the PLC software SIMATIC WinAC and the SIMATIC WinCC flexible visualization software.

  • Setup and function of a multi-core processor (single-core and dual-core systems).
  • Technical terms for Intel® Core™ 2 Duo.
  • Explanation of technical terms like Wide Dynamic Execution, Advanced Smart Cache and Smart Memory Access.
  • Operating modes of multi-core processors, asymmetric and symmetric multi-core processor systems, virtualization.
  • Intel® Core™ 2 Duo processors in SIMATIC PCs.
  • Overview of chip sets used, clock-pulse rates, power loss etc. for SIMATIC PCs.
  • Intel® Core™ 2 Duo processor technology with SIMATIC WinAC installation options for SIMATIC WinAC on SIMATIC PCs with Intel® Core™ 2 Duo processors (shared and dedicated mode).
  • Performance comparisons for SIMATIC WinAC RTX and SIMATIC WinCC flexible on an Intel® Core™ 2 Duo processor and a single-core processor:
    • CPU load
    • Update time
    • Picture opening time

A detailed description is available in the "White Paper – SIMATIC PC with Intel® Core™2 Duo" at the following link: White_Paper

 Entry ID:31939363   Date:2012-10-24 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour