show the entry list
WinCC -- Setting up development environments -- Installing / setting up operating systems
Why do other WinCC stations not appear in the network environment on the Windows 7 and Windows Server 2008 PCs?
Why should you not install the Microsoft security patches KB2467174, KB2467175, KB2465361 and KB2465367 in WinCC, PCS 7 and WinCC Professional V11?
What should you watch out for when using WinCC in a domain?
Which Microsoft Patches ("Security Patches" and "Critical Patches") have been tested for compatibility with SIMATIC WinCC?
What should you pay attention to when using WinCC with OEM operating systems?
How do you uninstall SP3 of Microsoft Windows XP?
Detailed information via the installed version of Microsoft Windows
Why can the WinCC uniclient not open the project from the server?
What restrictions are there for assigning the computer name for WinCC?
Logging off USB sticks from the operating system
How can you prevent Microsoft Windows Explorer from being opened as soon as you connect a USB stick to the computer or insert a CD/DVD in a drive?
How can you prevent the "Autoplay" function when inserting a CD/DVD or when connecting a USB device?
How do you uninstall SP3 of Microsoft Windows XP?
Part number:

Description:
If you have a PC with the operating system Microsoft Windows XP SP3 for WinCC and your version of WinCC is not released for the SP3 of Microsoft Windows XP, you must uninstall SP3 on your PC.

More information on compatibility between operating systems and WinCC is available in Entry ID: 21927773

Instructions:
How to uninstall Service Pack 3 of Windows XP Professional is described by Microsoft (www.microsoft.com) in Entry ID 950249 (direct link).

Keywords:
Service pack

 Entry ID:31694896   Date:2008-09-29 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour