show the entry list
S7-F-Systems -- Creating S7 programs -- Calling blocks and functions
Why does the Voter block F_2oo3_AI (FB317) no longer output the expected values after a delta deviation of all three process value inputs?
Where can you download the F FBs for the Mobile Panel 277F IWLAN for the Safety option of STEP 7 V5.5 and STEP 7 Professional V11?
How do you implement an Emergency Stop for stop categories 0 and 1?
Why should you close opened faceplates for a change of user (log on/off)?
What should you watch out for in large projects if you are using F module types?
What do you have to watch out for when upgrading Failsafe Blocks (V1_2) to S7 F Systems Lib V1_3?
What should you watch out for when evaluating the outputs V_MOD and AL_STATE of the F channel drivers F_CH_AI and F_PA_AI of the F systems library V1_3?
How can you acquire volumes error-free with SIMATIC F systems?
What should you watch out for in large projects if you are using F module types?
Part number:

Description
If the amount of F module parameters *.PAR_ID in a safety program exceeds the limit of 65535 and a part of the PAR_IDs is used for F module types, the overall signature of the safety program in the printout footer and in the program information part might differ. It might also happen that the safety mode can no longer be enabled after a delta load of the safety program.

When should you expect this behavior?
You should expect this behavior if all the following conditions apply:

  • Safety program created with F systems V5.2 or V6.0
  • Safety program contains F module types
  • Limit of 65535 PAR_IDs exceeded
  • Changes in the program incorporated with delta load

How can you prevent this behavior?
You can prevent this behavior by not exceeding the limit of 65535 PAR_IDs in your project. You can reduce the amount of PAR_IDs by:

  • Deleting F modules and F module types that are not required from the safety program
  • Reducing the amount of unused inputs and outputs to F module types (such as by creating a F_OR8 instead of a F_OR16)
  • Dividing the safety program across several F-CPUs.

Help tool
You can determine the amount of PAR_IDs by using "S7FPIdInfo.exe".
Use of "S7FPIdInfo.exe" is intuitive. Press the "Search" button to select the appropriate S7 program. Alternatively, you can drag the S7 program from the SIMATIC Manager to the "Search" button. The count procedure begins when you press the "Start" button. The amount of PAR_IDs of the S7 program is given under "Total". Select the relevant S7 program via the "Search" button again if you want to carry out more Par_ID count procedures.

Validity
The "S7FPIdInfo.exe" tool is only to be used in connection with F Systems V5.2 SP4 or V6.0.

Download

S7FPIdInfo_e.zip ( 478 KB )

Keywords:
Safety Integrated

 Entry ID:31411433   Date:2010-01-27 
I regard this article....as helpfulas not helpful                                 
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour