show the entry list
Sales/Delivery Release: SIMATIC Mobile Panel 277 10"
Summary Internet document

 

Effective immediately, the SIMATIC Mobile Panel 277 10" is available ex stock. With it, the family of the SIMATIC Mobile Panels is expanded by a 10.4" device in the 270 series performance class.     
 

Internet document Summary


The Mobile Panel 277 10" is distinguished by: 

  • 10.4" display with a resolution of 800 x 600 pixels 
  • Onboard safety functionality (enabling keys, STOP)
  • Touchscreen operation with touchscreen stylus fastener option at the rear of the enclosure 
  • Connectable to all standard Mobile Panel system components (connection boxes, connection cables)
  • Configurable from WinCC flexible 2008 Standard
  • Function scope corresponding to that of the Mobile Panel 277 8" 
  • Model with touchscreen (no function keys), STOP, and enabling keys 

The new device provides the advantages of a Mobile Panel in the 270 series performance class also with a larger display

  • Flexible in application at different connection points in conjunction with standard system components of the Mobile Panels 
  • Used when direct visual contact to the process is required, e.g., during precise setup or the exact adjustment of process parameters 

Therefore, projects for mobile applications can now also be implemented that for example: 

  • Require the quantity structure of the 270 series class 
  • Require a larger screen with high resolution 
  • Utilize scripts and archives

Effective immediately, the SIMATIC Mobile Panel 277 10" is available ex stock.
Object of the Release: SIMATIC Mobile Panel 277 10" DP/PN
Delivery Start: September 2008
Contacts: Contact: Siemens Partners on the Internet
Catalogs: CA01, ST80, A&D Mall
Internet Links: http://www.siemens.com/hmi-selection-tool
http://www.siemens.com/mobile-panels


The Mobile Panel 277 10" is offered in one equipment version (touchscreen with STOP and enabling keys). The connection to PROFIBUS or PROFINET is performed by connecting to the connection box DP or PN using the connection cable DP or PN.

( 44 KB )

 

SIMATIC Mobile Panel 277 10"

Product highlights of the Mobile Panel 277 10":

  • High-contrast 10" touchscreen display with a resolution of 800 x 600 pixels 
  • Configurable with WinCC flexible 2008 from version Standard 
  • Externally accessible USB port  
  • 6 MB flash user memory 
  • IP65 all-around, max. drop height of 1.0 m
  • Onboard safety functionality (enabling keys, STOP
  • Safety certification by SIBE 
  • Touchscreen stylus fastener option at the rear of the device
  • Support of scripts
  • Usage of archives
  • Non-volatile, maintenance-free alarm buffer
  • Pocket Internet Explorer for displaying HTML pages  

Ordering Data:
Product Name Order Number
Mobile Panel
Mobile Panel 277 10" DP/PN 6AV6 645-0BE02-0AX00


Accessories for the Mobile Panel 277 10"
Protective Film for SIMATIC Mobile Panel 277 10" to protect the Touchscreen Front against Dirt / Scratches (Set of 10, packed ready to ship) 6AV6645-7AB15-0AS0
Stylus for Touchscreen Operation incl. Fastener (Nylon String) for SIMATIC Mobile Panel 277 10" (Set of 5, packed ready to ship) 6AV6645-7AB14-0AS0


Documentation (free Download at !23342762!)
Operating Manual Mobile Panel 277, German 6AV6691-1DL01-0AA0
Operating Manual Mobile Panel 277, English 6AV6691-1DL01-0AB0
Operating Manual Mobile Panel 277, French 6AV6691-1DL01-0AC0
Operating Manual Mobile Panel 277, Italian 6AV6691-1DL01-0AD0
Operating Manual Mobile Panel 277, Spanish 6AV6691-1DL01-0AE0


 Entry ID:31011338   Date:2008-10-02 
I regard this article....as helpfulas not helpful                                 
related links
WinCC Comfort / WinCC Advanced V1 ...
SIMATIC HMI HMI device Mobile Pan ...
SIMATIC HMI HMI device Mobile Pa ...
mySupport
My Documentation Manager 
Newsletter 
CAx-Download-Manager 
Support Request
To this entry
Print
Create PDF 
Send to a friend
QuickLinks
Compatibility tool 
Help
Online Help
Guided Tour